Choose this feed adapter when you wish to convey small parts/particles, such as tablets or capsules: the bent design protects fragile materials during conveying. The feed adapter is used to add the optimum amount of air to the material flow. It is adjusted to the bottom of a feed station (when it is in use) or sieves, big bag stations, mixers, containers, or other equipment. It features an adjustable air inlet that helps control the conveying phase. If faster conveying is required and the material is not sensitive, dilute phase is needed. In the case of a delicate product, dense phase conveying has to be reached. The air inlets may be covered with Piab Air inlet filters when the risk of cross-contamination needs to be eliminated.
Läs mer Read less
Denna aktivitet kräver inloggning
logga in eller registrera för att få full nytta av piab.com
0
Olika produkttyper kan inte jämföras. Vill du ta bort befintliga produkter?