스테이지 4 업그레이드를 위한 비즈니스 사례 구축: 20개월간의 결정으로 20년간의 사고

2026. 9. 15.에 게시됨
4단계 폐수 업그레이드를 위한 비즈니스 사례

By the time you reach the decision stage, the technical analysis is usually clear. What stalls projects is alignment. 
Engineering wants the right solution. Operations wants something that will not consume their staff. Finance wants a defensible business case. Municipal leadership wants assurance that the plant will meet its compliance obligations under Directive (EU) 2024/3019 without operational surprises. 
This article gives you a structure that translates the fourth-stage decision into terms each of these stakeholders will recognize – and decision criteria that survive internal debate and future audits. 

Anchor the decision in a philosophy, not in components 

The most common trap at decision stage is to compare components line by line: pumps vs. pumps, silos vs. silos, dosing units vs. dosing units. That path leads to the "cheapest compliant option" – and often to an operationally fragile plant that consumes staff time for 20 years. 
Anchor the decision in a single sentence: 
"We will only invest in a fourth-stage solution that meets compliance reliably without requiring daily operator intervention – for 20 years." 

Three pillars for the business case 

Compliance reliability 
Directive (EU) 2024/3019 sets performance targets that must be met consistently, not just on average [1]. A dosing system that under-doses 5% of the time fails compliance 5% of the time. The business case must quantify the risk of compliance gaps – including reputational and regulatory exposure to the municipality. 

Lifecycle operating cost 

  • The procurement quote is a small fraction of the 20-year cost. Translate the decision into: 
  • PAC consumption over 20 years (the largest variable cost). 
  • Operator hours per week on the fourth stage. 
  • Maintenance and downtime hours per year. 
  • Energy demand (especially relevant for ozonation alternatives). 
  • Suppliers that offer 5% lower CAPEX but 20% higher consumable use will lose this comparison by a wide margin – if it is made. 


Workforce resilience 
Municipal water utilities face the same workforce pressure as private industry: fewer skilled operators, more shift turnover. A fourth-stage solution that requires expert intervention is a liability. One that runs reliably with standard staffing is an asset. 

Five non-negotiable criteria 

  • Documented dosing accuracy ±X% over 6+ months at comparable installations. 
  • Maximum operator intervention of Y hours per week under normal operation. 
  • Maintenance access without taking the dosing line offline for more than Z hours. 
  • Reference plants with PAC duty at comparable PE scale. 
  • Supplier track record on activated carbon dosing in adjacent industries (e.g. waste incineration). 

Score each shortlisted alternative against these criteria – not just against price and lead time. Document why options that looked attractive on paper were rejected. 

Why this is a 20-year decision 

The fourth stage will be a fixed part of your plant for the next two decades. Directive (EU) 2024/3019 is not the last regulatory step – the European Environment Agency has already flagged additional micropollutants as future regulatory candidates [5]. A flexible, robust fourth-stage platform will absorb future requirements. A fragile one will need to be partly rebuilt. 

What to do next 

Bring engineering, operations, and finance into the same room with the criteria above. The output should be a single, defensible recommendation – with a clear paper trail of how alternatives were evaluated and why the chosen solution is the responsible choice for the next 20 years.

For background that helps non-specialist stakeholders, you can link to the explainers "What does "PE" mean in a wastewater treatment plant?", "Activated carbon vs. ozonation – a quick comparison for fourth-stage planning", and "Why powdered activated carbon is difficult to handle and dose reliably". 

Discover more insights

Insights
2026. 11. 11.

분말 취급: 변경 사항 및 적응 방법

대부분의 플랜트에서 분말 이송은 무언가가 멈출 때만 주목을 받습니다. 펌프, 필터 및 분체이송기는 백그라운드에서 작동하며, 한 번 사양이 정해지면 그대로 방치됩니다. 이러한 관행이 변하고 있습니다. 변화를 주도하는 요인과 차세대 이송 장비가 갖춰야 할 요소를 알아보세요.
분말 취급: 변경 사항 및 적응 방법
Insights
2026. 11. 11.

생산 라인의 PFAS: 공정 장비에 대한 EU 제한의 의미

PFAS에 대한 대부분의 대화는 붙지 않는 프라이팬과 아웃도어 재킷과 같은 소비재에 중점을 둡니다. 그러나 PFAS는 씰, 개스킷, 코팅 및 필터 매체와 같은 산업 장비에도 내장되어 있습니다. 생산 현장을 책임지는 모든 사람에게 있어 문제는 더 이상 PFAS의 규제 여부가 아니라 장비와 공급망이 얼마나 빨리 적응할 수 있느냐 하는 것입니다.
생산 라인의 PFAS: 공정 장비에 대한 EU 제한의 의미
Insights
2026. 11. 11.

추측에서 제어까지: 분말 진공이송에서 예비부품 추적성이 중요한 이유

많은 생산공정에서 예비 부품 지식은 사람들의 머리, 마모된 라벨 및 구순서 확인에 존재합니다. 누군가가 떠나거나, 라벨이 희미해지거나, 감사관이 아무도 대답할 수 없는 질문을 할 때까지 작동합니다. 운영 리더의 경우, 이는 유지 보수 세부 사항이 아닌 제어 문제입니다.
추측에서 제어까지: 분말 진공이송에서 예비부품 추적성이 중요한 이유
Insights
2026. 11. 11.

파이아브 (Piab) 의 소결 필터로 업그레이드하기 위한 비즈니스 사례

ot; 수백 번의 테스트를 실행했지만 파손을 시뮬레이션할 수 없었습니다.
파이아브 (Piab) 의 소결 필터에 대한 비즈니스 사례: 추적성, 규정 준수 및 제어
Insights
2026. 9. 15.

EU 지침 2024/3019: 네 번째 처리 스테이지가 플랜트에 미치는 영향

EU 폐수 지침 2024/3019: 4차 처리 스테이지
View all

Do you need help choosing the right product?

Get free advice from our engineers

국가
최신 뉴스를 받고 싶습니다
이송 솔루션

기사 공유