분말 활성탄이 다루기 어렵고 안정적으로 투여되는 이유

2026. 9. 15.에 게시됨
분말 활성탄이 다루기 어렵고 안정적으로 투여되는 이유

Powdered activated carbon (PAC) is one of the more demanding bulk powders to handle in a wastewater plant. It is very fine, cohesive, and electrostatically active, which makes it prone to bridging, rat‑holing, dust formation, and unstable flow in small feeders. These bulk‑handling effects show up directly in the dosing system: surging, starving, or frequent operator interventions. 

When PAC is added to the aeration or contact tank, operators sometimes also talk about a “cocoa effect”: PAC floating and clumping on the water surface before it fully wets and sinks. That in‑tank behaviour is mainly a mixing and hydrodynamics issue. Bulk material handling and dosing cannot remove the cocoa effect, but stable, accurate dosing and a well‑controlled injection point make it easier for the plant’s mixing system to do its job. 

 
In a wastewater treatment plant, this is not a cosmetic problem. The fourth treatment stage relies on a precise dose of activated carbon to adsorb micropollutants. Under-dosing means micropollutants pass through; over-dosing wastes a significant operating cost.

Why PAC is particularly difficult 

  • It is extremely fine (typical particle size 10–50 µm), which makes it cohesive and prone to bridging. 
  • It is hygroscopic – it absorbs moisture from the air, which makes it clump. 
  • It carries electrostatic charge, which makes it stick to internal surfaces and form buildup over time. 

These powder properties sit behind the dry‑side bulk‑handling challenges and also influence how PAC behaves once it enters the aeration or contact tank. 

How robust dosing systems address it 

Modern dosing solutions designed for PAC combine several principles: vacuum or low-pressure conveying that avoids the compaction caused by mechanical screws; geometry that minimizes dead zones and surface contact; controlled aeration or fluidization at the discharge point; and clean-in-place features that prevent gradual buildup from changing dose accuracy over time. 
The difference between a system designed for "carbon-like powders in general" and one designed specifically for PAC at full-scale plant duty is often the difference between a fourth-stage plant that runs reliably and one that requires daily intervention.

Why it matters for procurement 

In the procurement phase, bulk‑handling behaviour is often underestimated – yet it is one of the single largest sources of operating risk in fourth‑stage plants. The critical point is not whether the system doses “continuously” at very small rates, but whether it can dose accurately and repeatably at the dosing regime chosen for the process (continuous or discontinuous). 
Asking vendors for documented dosing accuracy over 6–12 months of continuous operation, not just commissioning data, is one of the most effective ways to surface this risk early. 

This explainer is referenced from the articles "Activated carbon or ozonation? A framework for choosing your fourth-stage technology" and "Building the business case for a fourth-stage upgrade: 20-year thinking in a 20-month decision"

Discover more insights

Insights
2026. 11. 11.

분말 취급: 변경 사항 및 적응 방법

대부분의 플랜트에서 분말 이송은 무언가가 멈출 때만 주목을 받습니다. 펌프, 필터 및 분체이송기는 백그라운드에서 작동하며, 한 번 사양이 정해지면 그대로 방치됩니다. 이러한 관행이 변하고 있습니다. 변화를 주도하는 요인과 차세대 이송 장비가 갖춰야 할 요소를 알아보세요.
분말 취급: 변경 사항 및 적응 방법
Insights
2026. 11. 11.

생산 라인의 PFAS: 공정 장비에 대한 EU 제한의 의미

PFAS에 대한 대부분의 대화는 붙지 않는 프라이팬과 아웃도어 재킷과 같은 소비재에 중점을 둡니다. 그러나 PFAS는 씰, 개스킷, 코팅 및 필터 매체와 같은 산업 장비에도 내장되어 있습니다. 생산 현장을 책임지는 모든 사람에게 있어 문제는 더 이상 PFAS의 규제 여부가 아니라 장비와 공급망이 얼마나 빨리 적응할 수 있느냐 하는 것입니다.
생산 라인의 PFAS: 공정 장비에 대한 EU 제한의 의미
Insights
2026. 11. 11.

추측에서 제어까지: 분말 진공이송에서 예비부품 추적성이 중요한 이유

많은 생산공정에서 예비 부품 지식은 사람들의 머리, 마모된 라벨 및 구순서 확인에 존재합니다. 누군가가 떠나거나, 라벨이 희미해지거나, 감사관이 아무도 대답할 수 없는 질문을 할 때까지 작동합니다. 운영 리더의 경우, 이는 유지 보수 세부 사항이 아닌 제어 문제입니다.
추측에서 제어까지: 분말 진공이송에서 예비부품 추적성이 중요한 이유
Insights
2026. 11. 11.

파이아브 (Piab) 의 소결 필터로 업그레이드하기 위한 비즈니스 사례

ot; 수백 번의 테스트를 실행했지만 파손을 시뮬레이션할 수 없었습니다.
파이아브 (Piab) 의 소결 필터에 대한 비즈니스 사례: 추적성, 규정 준수 및 제어
Insights
2026. 9. 15.

EU 지침 2024/3019: 네 번째 처리 스테이지가 플랜트에 미치는 영향

EU 폐수 지침 2024/3019: 4차 처리 스테이지
View all

Do you need help choosing the right product?

Get free advice from our engineers

국가
최신 뉴스를 받고 싶습니다
이송 솔루션

기사 공유