EU 지침 2024/3019: 네 번째 처리 스테이지가 플랜트에 미치는 영향

2026. 9. 15.에 게시됨
EU 지침 2024/3019: 네 번째 처리 스테이지가 플랜트에 미치는 영향

Since the entry into force of Directive (EU) 2024/3019 on urban wastewater treatment, European wastewater operators have been on a clock. Every treatment plant serving more than 150,000 population equivalents (PE) must be equipped with a quaternary – fourth – treatment stage, with phased deadlines extending to 2045. 
For many plant operators, the implications are still settling in. This article explains what is changing, why, and what plant managers should be thinking about now – well before procurement begins.


Why a fourth stage is needed 

The three conventional treatment stages – mechanical, biological, and chemical – remove solids, organic load, and nutrients effectively. What they cannot reliably remove are micropollutants: pharmaceutical residues, contrast agents used in medical imaging, hormones, and a wide range of other trace contaminants. 
These substances pass through conventional treatment unchanged and reach surface waters in measurable concentrations. The OECD has identified pharmaceutical residues in freshwater as a growing risk to aquatic ecosystems and, indirectly, to drinking water sources. The European Environment Agency reports detectable levels of pharmaceuticals in surface waters across all member states surveyed. 
The fourth stage is designed specifically to capture these substances – typically through adsorption on activated carbon or oxidation processes such as ozonation. 


What the directive requires 

The directive applies to all urban wastewater treatment plants serving more than 150,000 PE. 
Member states must achieve full implementation by 2045, with intermediate milestones starting in 2033. 
In Germany alone, roughly 10,000 wastewater treatment plants are in operation, of which approximately 3,000 fall within scope and must be upgraded. 
Other European countries face proportionally similar obligations as they translate the directive into national law. 


Why this is a strategic decision, not just a technical one 

For plant managers and municipal operators, the fourth stage is one of the largest capital investments most plants will make this decade. The decisions made now will shape operating cost, staffing requirements, and compliance posture for 20 years or more.

Three questions deserve early attention: 
Which adsorbent or process fits your influent profile? Activated carbon is the most common choice and is well understood, but dosing reliability varies dramatically between providers. 

How will the dosing system behave in daily operation? Powdered activated carbon presents real handling challenges especially in the dry bulk handling and dosing step: bridging and ratholing in silos and hoppers, unstable flow in very small feeders, dust and gradual buildup on internal surfaces. In the aeration or contact tank, many operators also describe a “cocoa effect” – PAC floating and clumping on the water surface before it fully wets and sinks – but that in‑tank behaviour is mainly a question of mixing and tank design, not something the bulk material handling alone can remove. 


What is the operational complexity over 20 years? Some fourth-stage solutions are technically complete but operationally fragile. Others prioritize robustness and simplicity. The difference shows up not in the procurement quote, but in the lifecycle cost. 


What to do next 

If your plant is above the 150,000 PE threshold – or close to it – the time to start scoping is now, not when the deadline approaches. Early movers have access to better engineering support, more flexible budgeting, and the ability to learn from pilot installations before committing. 

For a quick reference on core concepts mentioned here, see the explainer "What does "PE" mean in a wastewater treatment plant?" and "Activated carbon vs. ozonation – a quick comparison for fourth-stage planning". 
Next in the series: how to compare activated carbon vs. ozonation, and what to look for in a dosing system that has to run reliably for 20 years.

Discover more insights

Insights
2026. 11. 11.

분말 취급: 변경 사항 및 적응 방법

대부분의 플랜트에서 분말 이송은 무언가가 멈출 때만 주목을 받습니다. 펌프, 필터 및 분체이송기는 백그라운드에서 작동하며, 한 번 사양이 정해지면 그대로 방치됩니다. 이러한 관행이 변하고 있습니다. 변화를 주도하는 요인과 차세대 이송 장비가 갖춰야 할 요소를 알아보세요.
분말 취급: 변경 사항 및 적응 방법
Insights
2026. 11. 11.

생산 라인의 PFAS: 공정 장비에 대한 EU 제한의 의미

PFAS에 대한 대부분의 대화는 붙지 않는 프라이팬과 아웃도어 재킷과 같은 소비재에 중점을 둡니다. 그러나 PFAS는 씰, 개스킷, 코팅 및 필터 매체와 같은 산업 장비에도 내장되어 있습니다. 생산 현장을 책임지는 모든 사람에게 있어 문제는 더 이상 PFAS의 규제 여부가 아니라 장비와 공급망이 얼마나 빨리 적응할 수 있느냐 하는 것입니다.
생산 라인의 PFAS: 공정 장비에 대한 EU 제한의 의미
Insights
2026. 11. 11.

추측에서 제어까지: 분말 진공이송에서 예비부품 추적성이 중요한 이유

많은 생산공정에서 예비 부품 지식은 사람들의 머리, 마모된 라벨 및 구순서 확인에 존재합니다. 누군가가 떠나거나, 라벨이 희미해지거나, 감사관이 아무도 대답할 수 없는 질문을 할 때까지 작동합니다. 운영 리더의 경우, 이는 유지 보수 세부 사항이 아닌 제어 문제입니다.
추측에서 제어까지: 분말 진공이송에서 예비부품 추적성이 중요한 이유
Insights
2026. 11. 11.

파이아브 (Piab) 의 소결 필터로 업그레이드하기 위한 비즈니스 사례

ot; 수백 번의 테스트를 실행했지만 파손을 시뮬레이션할 수 없었습니다.
파이아브 (Piab) 의 소결 필터에 대한 비즈니스 사례: 추적성, 규정 준수 및 제어
Insights
2026. 9. 15.

EU 지침 2024/3019: 네 번째 처리 스테이지가 플랜트에 미치는 영향

EU 폐수 지침 2024/3019: 4차 처리 스테이지
View all

Do you need help choosing the right product?

Get free advice from our engineers

국가
최신 뉴스를 받고 싶습니다
이송 솔루션

기사 공유