Ir al contenido

Does an ejector pump use more energy than a mechanical pump?

When the pumps are on, the vacuum ejector pump actually uses more energy than the mechanical, however most vacuum applications are intermittent- suction and release- and the ejector pump can follow that cycle and be switched off and on easily along with the cycle which in total gives a much lower energy consumption compared to the mechanical pump that is on all the time.