Ir al contenido

What can go wrong with the unit?

With regular maintenance, the vacuum conveyor unit will do the job for years to come.

If the compressed air is dirty/has fluid in it, the filter can be clogged as well as the ejectors and the timers. Water in the air line is not optimal.

Consult the manual for troubleshooting if you would encounter anything unusual.