Elaboração do estudo de viabilidade para uma modernização de quarto estágio: uma visão de 20 anos em uma decisão de 20 meses

Publicado 15/09/2026
Argumentação comercial para uma modernização de tratamento de águas residuais de quarto estágio

By the time you reach the decision stage, the technical analysis is usually clear. What stalls projects is alignment. 
Engineering wants the right solution. Operations wants something that will not consume their staff. Finance wants a defensible business case. Municipal leadership wants assurance that the plant will meet its compliance obligations under Directive (EU) 2024/3019 without operational surprises. 
This article gives you a structure that translates the fourth-stage decision into terms each of these stakeholders will recognize – and decision criteria that survive internal debate and future audits. 

Anchor the decision in a philosophy, not in components 

The most common trap at decision stage is to compare components line by line: pumps vs. pumps, silos vs. silos, dosing units vs. dosing units. That path leads to the "cheapest compliant option" – and often to an operationally fragile plant that consumes staff time for 20 years. 
Anchor the decision in a single sentence: 
"We will only invest in a fourth-stage solution that meets compliance reliably without requiring daily operator intervention – for 20 years." 

Three pillars for the business case 

Compliance reliability 
Directive (EU) 2024/3019 sets performance targets that must be met consistently, not just on average [1]. A dosing system that under-doses 5% of the time fails compliance 5% of the time. The business case must quantify the risk of compliance gaps – including reputational and regulatory exposure to the municipality. 

Lifecycle operating cost 

  • The procurement quote is a small fraction of the 20-year cost. Translate the decision into: 
  • PAC consumption over 20 years (the largest variable cost). 
  • Operator hours per week on the fourth stage. 
  • Maintenance and downtime hours per year. 
  • Energy demand (especially relevant for ozonation alternatives). 
  • Suppliers that offer 5% lower CAPEX but 20% higher consumable use will lose this comparison by a wide margin – if it is made. 


Workforce resilience 
Municipal water utilities face the same workforce pressure as private industry: fewer skilled operators, more shift turnover. A fourth-stage solution that requires expert intervention is a liability. One that runs reliably with standard staffing is an asset. 

Five non-negotiable criteria 

  • Documented dosing accuracy ±X% over 6+ months at comparable installations. 
  • Maximum operator intervention of Y hours per week under normal operation. 
  • Maintenance access without taking the dosing line offline for more than Z hours. 
  • Reference plants with PAC duty at comparable PE scale. 
  • Supplier track record on activated carbon dosing in adjacent industries (e.g. waste incineration). 

Score each shortlisted alternative against these criteria – not just against price and lead time. Document why options that looked attractive on paper were rejected. 

Why this is a 20-year decision 

The fourth stage will be a fixed part of your plant for the next two decades. Directive (EU) 2024/3019 is not the last regulatory step – the European Environment Agency has already flagged additional micropollutants as future regulatory candidates [5]. A flexible, robust fourth-stage platform will absorb future requirements. A fragile one will need to be partly rebuilt. 

What to do next 

Bring engineering, operations, and finance into the same room with the criteria above. The output should be a single, defensible recommendation – with a clear paper trail of how alternatives were evaluated and why the chosen solution is the responsible choice for the next 20 years.

For background that helps non-specialist stakeholders, you can link to the explainers "What does "PE" mean in a wastewater treatment plant?", "Activated carbon vs. ozonation – a quick comparison for fourth-stage planning", and "Why powdered activated carbon is difficult to handle and dose reliably". 

Discover more insights

Insights
30/10/2026

PFAS na sua linha de produção: o que a restrição da UE significa para os equipamentos de processo

A maioria das discussões sobre PFAS concentra-se em produtos de consumo, como panelas antiaderentes e jaquetas para atividades ao ar livre. Mas os PFAS também estão presentes em equipamentos industriais: vedações, juntas, revestimentos e meios filtrantes. Para qualquer pessoa responsável por uma unidade de produção, a questão já não é se os PFAS serão regulamentados, mas sim com que rapidez seus equipamentos e sua cadeia de suprimentos poderão se adaptar.
PFAS em sua linha de produção: o que a restrição da UE significa para os equipamentos de processo
Insights
30/10/2026

Da suposição ao controle: por que a rastreabilidade de peças sobressalentes é importante na manipulação de pó

Em muitas fábricas, o conhecimento sobre peças sobressalentes fica na cabeça das pessoas, em rótulos desgastados e em antigas confirmações de pedidos. Isso funciona até que alguém saia da empresa, um rótulo desbote ou um auditor faça uma pergunta que ninguém saiba responder. Para um líder de operação, isso é um problema de controle, não um detalhe de manutenção.
Da suposição ao controle: por que a rastreabilidade de peças sobressalentes é importante na manipulação de pó
Insights
30/10/2026

Os argumentos comerciais para a migração para o filtro sinterizado da Piab

“Realizamos centenas de testes, mas não conseguimos simular uma quebra.” Essa é uma frase do nosso vídeo, mas a robustez é apenas parte da história. Para as áreas de operações e compras, as verdadeiras questões são: o que um filtro oferece em termos de controle, conformidade e produtividade, e quanto esforço é necessário para fazer a troca. Veja a seguir como o filtro sinterizado responde a cada uma delas.
O caso de negócios do filtro sinterizado da Piab: rastreabilidade, conformidade e controle
Insights
30/10/2026

Transporte de pó: o que está mudando e como se adaptar

Na maioria das fábricas, o transporte de pó só recebe atenção quando algo para de funcionar. A bomba, o filtro e o transportador funcionam em segundo plano, configurados uma vez e deixados de lado. Esse hábito está mudando. Descubra o que está impulsionando a mudança e o que a próxima geração de equipamentos de transporte precisa oferecer.
Transporte de pós: o que está mudando e como se adaptar
Insights
15/09/2026

Quando a manipulação de alimentos em pó sobrecarrega sua equipe e sua linha de produção

Manipulação de alimentos em pó: reduzindo a sobrecarga e as interrupções na linha de produção
View all

Do you need help choosing the right product?

Get free advice from our engineers

País
Eu quero receber as últimas notícias sobre
Soluções de transporte

Compartilhar artigo