Diretiva da UE 2024/3019: o que o quarto estágio de tratamento significa para a sua estação

Publicado 15/09/2026
Diretiva da UE 2024/3019: o que o quarto estágio de tratamento significa para a sua estação

Since the entry into force of Directive (EU) 2024/3019 on urban wastewater treatment, European wastewater operators have been on a clock. Every treatment plant serving more than 150,000 population equivalents (PE) must be equipped with a quaternary – fourth – treatment stage, with phased deadlines extending to 2045. 
For many plant operators, the implications are still settling in. This article explains what is changing, why, and what plant managers should be thinking about now – well before procurement begins.


Why a fourth stage is needed 

The three conventional treatment stages – mechanical, biological, and chemical – remove solids, organic load, and nutrients effectively. What they cannot reliably remove are micropollutants: pharmaceutical residues, contrast agents used in medical imaging, hormones, and a wide range of other trace contaminants. 
These substances pass through conventional treatment unchanged and reach surface waters in measurable concentrations. The OECD has identified pharmaceutical residues in freshwater as a growing risk to aquatic ecosystems and, indirectly, to drinking water sources. The European Environment Agency reports detectable levels of pharmaceuticals in surface waters across all member states surveyed. 
The fourth stage is designed specifically to capture these substances – typically through adsorption on activated carbon or oxidation processes such as ozonation. 


What the directive requires 

The directive applies to all urban wastewater treatment plants serving more than 150,000 PE. 
Member states must achieve full implementation by 2045, with intermediate milestones starting in 2033. 
In Germany alone, roughly 10,000 wastewater treatment plants are in operation, of which approximately 3,000 fall within scope and must be upgraded. 
Other European countries face proportionally similar obligations as they translate the directive into national law. 


Why this is a strategic decision, not just a technical one 

For plant managers and municipal operators, the fourth stage is one of the largest capital investments most plants will make this decade. The decisions made now will shape operating cost, staffing requirements, and compliance posture for 20 years or more.

Three questions deserve early attention: 
Which adsorbent or process fits your influent profile? Activated carbon is the most common choice and is well understood, but dosing reliability varies dramatically between providers. 

How will the dosing system behave in daily operation? Powdered activated carbon presents real handling challenges especially in the dry bulk handling and dosing step: bridging and ratholing in silos and hoppers, unstable flow in very small feeders, dust and gradual buildup on internal surfaces. In the aeration or contact tank, many operators also describe a “cocoa effect” – PAC floating and clumping on the water surface before it fully wets and sinks – but that in‑tank behaviour is mainly a question of mixing and tank design, not something the bulk material handling alone can remove. 


What is the operational complexity over 20 years? Some fourth-stage solutions are technically complete but operationally fragile. Others prioritize robustness and simplicity. The difference shows up not in the procurement quote, but in the lifecycle cost. 


What to do next 

If your plant is above the 150,000 PE threshold – or close to it – the time to start scoping is now, not when the deadline approaches. Early movers have access to better engineering support, more flexible budgeting, and the ability to learn from pilot installations before committing. 

For a quick reference on core concepts mentioned here, see the explainer "What does "PE" mean in a wastewater treatment plant?" and "Activated carbon vs. ozonation – a quick comparison for fourth-stage planning". 
Next in the series: how to compare activated carbon vs. ozonation, and what to look for in a dosing system that has to run reliably for 20 years.

Discover more insights

Insights
30/10/2026

PFAS na sua linha de produção: o que a restrição da UE significa para os equipamentos de processo

A maioria das discussões sobre PFAS concentra-se em produtos de consumo, como panelas antiaderentes e jaquetas para atividades ao ar livre. Mas os PFAS também estão presentes em equipamentos industriais: vedações, juntas, revestimentos e meios filtrantes. Para qualquer pessoa responsável por uma unidade de produção, a questão já não é se os PFAS serão regulamentados, mas sim com que rapidez seus equipamentos e sua cadeia de suprimentos poderão se adaptar.
PFAS em sua linha de produção: o que a restrição da UE significa para os equipamentos de processo
Insights
30/10/2026

Da suposição ao controle: por que a rastreabilidade de peças sobressalentes é importante na manipulação de pó

Em muitas fábricas, o conhecimento sobre peças sobressalentes fica na cabeça das pessoas, em rótulos desgastados e em antigas confirmações de pedidos. Isso funciona até que alguém saia da empresa, um rótulo desbote ou um auditor faça uma pergunta que ninguém saiba responder. Para um líder de operação, isso é um problema de controle, não um detalhe de manutenção.
Da suposição ao controle: por que a rastreabilidade de peças sobressalentes é importante na manipulação de pó
Insights
30/10/2026

Os argumentos comerciais para a migração para o filtro sinterizado da Piab

“Realizamos centenas de testes, mas não conseguimos simular uma quebra.” Essa é uma frase do nosso vídeo, mas a robustez é apenas parte da história. Para as áreas de operações e compras, as verdadeiras questões são: o que um filtro oferece em termos de controle, conformidade e produtividade, e quanto esforço é necessário para fazer a troca. Veja a seguir como o filtro sinterizado responde a cada uma delas.
O caso de negócios do filtro sinterizado da Piab: rastreabilidade, conformidade e controle
Insights
30/10/2026

Transporte de pó: o que está mudando e como se adaptar

Na maioria das fábricas, o transporte de pó só recebe atenção quando algo para de funcionar. A bomba, o filtro e o transportador funcionam em segundo plano, configurados uma vez e deixados de lado. Esse hábito está mudando. Descubra o que está impulsionando a mudança e o que a próxima geração de equipamentos de transporte precisa oferecer.
Transporte de pós: o que está mudando e como se adaptar
Insights
15/09/2026

Quando a manipulação de alimentos em pó sobrecarrega sua equipe e sua linha de produção

Manipulação de alimentos em pó: reduzindo a sobrecarga e as interrupções na linha de produção
View all

Do you need help choosing the right product?

Get free advice from our engineers

País
Eu quero receber as últimas notícias sobre
Soluções de transporte

Compartilhar artigo