Aller au contenu

Un boîtier de commande est-il fourni avec l'appareil ?

The unit has a pneumatic control which controls the suction and discharge time.

It can also be w/o control, in that case the end user will need to provide the sequence of operation – PLC control.

El/pneumatic valve unit can be provided (to convert the electrical signal to a pneumatic output to signal the Piab).