Feedback

Elige tu idioma

Cerrar

Why should I use an ejector pump instead of a mechanical pump?

The ejector technology has no moving parts thus  with virtually no maintenance, it will provide higher reliability. It is also much smaller in size and weight that gives you the possibility to place it closer to the point of suction or where you actually need the vacuum.  The mechanical pump also has a much higher noise level and produces heat, meaning that normally you would need to have it in an insulated room. 

Piab AB © 2020 Política de privacidad

Síguenos

Contáctenos