Feedback

Choose your language

Close

PR UpgradeKitConveyor

Extend the lifetime of your Piab C series vacuum conveyor

Date 25/03/2013

Simple upgrade

Piab, a leading supplier of industrial vacuum technology, introduces an upgrade kit for its C series vacuum conveyors.

This is a straightforward upgrade due to a standard interface between the C Series conveyor and the new piFLOW®p conveyor. The upgrade consists of a new COAX® powered vacuum pump called piPREMIUM, along with a cover, shock tank and control valve. The upgrade just snaps on to the existing C series conveyor with no tools needed.

Users benefit from the latest in vacuum technology from COAX®'s efficient design that saves on compressed air energy costs. The working environment is improved with a lower noise level from an integrated silencer. Uptime is increased with a maintenance-friendly design of less internal parts, one connection point. Its hygienic aspects provide for easy dismounting of parts and cleaning. Apart from all the new technical benefits that will be acquired with the upgrade – all other components can still be used, which is both economically and environmentally beneficial.

With a low investment, the conveyor will be able to meet future demands by adding additional capacity with the new modular piPREMIUM pump.

About Piab

Established in 1951, Piab designs innovative vacuum solutions that improve the energy-efficiency, productivity, and working environments of vacuum users around the world. As a reliable partner to many of the world's largest manufacturers, Piab develops and manufactures a complete line of vacuum pumps, vacuum accessories, vacuum conveyors and suction cups for a variety of automated material handling and factory automation processes. Piab utilizes COAX®, a completely new dimension in vacuum technology, in many of its original products and solutions. COAX® cartridges are smaller, more energy efficient and more reliable than conventional ejectors, and can be integrated directly into machinery. This allows for the design of a flexible, modular vacuum system. Piab is a worldwide organization with subsidiaries and distributors in more than 50 countries. Its headquarters are in Sweden.

More information

Häla El Sheemy Washbrook, Vice President Marketing and Communications Manager
Tel: +46 (0) 8 630 25 74
E-mail: hala.e.washbrook@piab.com

Piab AB © 2020 Privacy notice

Follow us

Contact us