Feedback

Choose your language

Close

piFLOW®t tablet conveyor

Dedicatedly gentle conveying of delicate food

Date 22/02/2017

Revolutionary flow control ensures a gentle touch in Piab's conveyor for fragile goods.

Taby, Sweden – Successfully solving the problems of using vacuum technology to convey the delicacies of the food industry, such as nuts, seeds, beans, candy, as well as nutraceutical tablets and capsules, Piab’s piFLOW®t conveyor is dedicated to the gentle handling of delicate ingredients and products. Promising to revolutionise the automated handling of fragile goods, the piFLOW®t features innovative and groundbreaking new technology (patent pending).

“A controlled low speed, guided entry into the conveyor, and the elimination of all sharp edges are the keys to our success, ensuring that products are handled with great care in our conveyors. There will be no more chipped candy in plants using piFLOW®t,” states Jarno Tahvanainen, Vice President of Piab’s Material Handling division.

Suitable for transporting up to four million items per hour, the piFLOW®t conveyor can be used to transport any fragile goods within a processing plant. For the food industry this enables the safe handling of, for instance, coated sweets, candy, roasted coffee beans, whole nuts, and nutraceutical tablets.

Eliminating the use of inadequate standard equipment and alternative, often back-breaking, manual procedures, piFLOW®t will safely transfer ingredients and products between the various processing units, such as tablet presses, coating drums, and packaging lines, avoiding all risks of damage.

At the core of piFLOW®t is the proprietary piGENTLE® an innovative technology (patent pending) that maintains a gentle flow by regulating the feed pressure of the pump, ensuring that fragile ingredients or products are handled as delicately as possible. piFLOW®t is an extension to Piab’s popular and high quality range of piFLOW® conveyors for powder and bulk materials, and is specially developed to meet the stringent demands regarding operational safety and hygiene within the food (piFLOW®f), pharmaceutical (piFLOW®p), and chemical (piFLOW®i) industries.

Contact us to conduct a lab test of your fragile goods.

About Piab

Established in 1951, Piab designs innovative vacuum solutions that improve the energy-efficiency, productivity, and working environments of vacuum users around the world. As a reliable partner to many of the world's largest manufacturers, Piab develops and manufactures a complete line of vacuum pumps, vacuum accessories, vacuum conveyors and suction cups for a variety of automated material handling and factory automation processes. Piab utilizes COAX®, a completely new dimension in vacuum technology, in many of its original products and solutions. COAX® cartridges are smaller, more energy efficient and more reliable than conventional ejectors, and can be integrated directly into machinery. This allows for the design of a flexible, modular vacuum system. In 2016, Piab completed two strategically important acquisitions, Kenos and Vaculex. Piab is a worldwide organization with subsidiaries and distributors in almost 70 countries. Its headquarters are in Sweden.

More information

Häla El Sheemy Washbrook, Vice President Marketing and Communications Manager
Tel: +46 (0) 8 630 25 74
E-mail: hala.e.washbrook@piab.com

Piab AB © 2020 Privacy notice

Follow us

Contact us