Activated carbon or ozonation? A framework for choosing your fourth-stage technology

Published 04/08/2026
Activated carbon or ozonation? A framework for choosing your fourth-stage technology

If you have established that your plant falls within the scope of Directive (EU) 2024/3019, the next question is technology. The directive deliberately does not prescribe a specific solution – it sets a performance target and leaves the choice to operators. 
This article gives you a structured way to compare the two dominant fourth-stage technologies – activated carbon adsorption and ozonation – and a framework for evaluating not just the technology itself, but the operational reality of running it for 20 years. 

The two technologies side by side 

Activated carbon (PAC or GAC) 
How it works: micropollutants adsorb onto the high surface area of the carbon. 
Strengths: broad spectrum of micropollutants captured, low energy demand, no harmful by-products, well-established design guidelines. 
Weaknesses: ongoing consumable cost; dosing reliability depends on robust powder handling; spent carbon must be disposed of or regenerated. 
Ozonation 
How it works: ozone oxidizes micropollutants directly in the water. 
Strengths: no continuous consumable to dose; compact footprint. 
Weaknesses: high electricity demand; can form by-products (such as bromate) requiring a downstream biological filter; more complex process control. 
A growing number of plants combine both – ozonation followed by activated carbon polishing, or activated carbon as the main stage with ozone reserved for specific contaminants.

The hidden decision: powder handling 

Most published comparisons stop at the technology level. But for plants choosing activated carbon, the real operational risk lies one step down: how reliably can the carbon actually be dosed?

Powdered activated carbon (PAC) is fine (10–50 µm), cohesive, hygroscopic, and electrostatically active. On the dry side, these properties cause exactly the bulk‑handling problems you see in practice: bridging and ratholing in silos and hoppers, feeders that struggle at very low throughputs, dust and residue on internal surfaces. In the aeration or contact tank, the same powder can also show a “cocoa effect” – PAC floating and clumping on the surface before it fully wets and sinks – but that in‑water behaviour is primarily about mixing and tank hydrodynamics, not about the bulk‑handling equipment itself. 
 
Under‑dosing or because the dry system bridges or starves, or over-dosing because the system surges, can both compromise the fourth‑stage performance. Even if the chemistry and tank are correctly designed, unstable dry‑side handling will show up as inconsistent removal. 
 
“What really matters is dosing accuracy in the chosen regime,” says Florian Stiller, technical expert at IB (Sales Support). “With long retention times in the aeration tank, robust discontinuous dosing of precisely defined batches is often more reliable than trying to run extremely small continuous flows through very delicate devices.” 

A framework for evaluating dosing systems 

1. Dosing accuracy over time, not just at commissioning.  

Dosing accuracy over time, not just at commissioning. Whether your process uses continuous or discontinuous PAC addition, the key is dose accuracy and repeatability at the dosing regime you choose – not the smallest possible continuous rate. Ask for documented dose accuracy over 6–12 months of operation. Commissioning data alone does not reveal how the system behaves once PAC has built up on internal surfaces. 

2. Containment and dust control. PAC dust is a housekeeping and health risk. A robust dosing system should keep the powder contained from delivery to dosing point without operator intervention. 
3. Cleaning and maintenance access. Buildup is inevitable. The question is how easily it can be removed without taking the dosing line offline for extended periods.

What decision-grade evidence looks like 

  • When you collect references and trial data at this stage, look for: 
  • Documented dosing accuracy (±%) over an extended operating period. 
  • Intervention frequency – how often operators have to step in during normal operation. 
  • Maintenance hours per year on the dosing system. 
  • Evidence that PAC reaches the injection point as intended (no chronic bridging, no uncontrolled surges), so that the plant’s mixing and tank design can deliver the desired dispersion. 

If a supplier cannot provide this, you do not yet have the information you need to decide. 

What to do next 

Use this framework internally with your engineering and operations teams. The output should be a shortlist of two to three solutions where the technology choice is settled and the remaining decision is about supplier robustness and lifecycle cost. 

For more background on the core technologies and operational risks discussed here, see the explainers "Activated carbon vs. ozonation – a quick comparison for fourth-stage planning" and "Why powdered activated carbon is difficult to handle and dose reliably".

Next in the series: how to translate this into a defensible business case for management and finance. 

Discover more insights

Insights
27/10/2026

Powder conveying: what’s changing and how to adapt

In most plants, powder conveying only gets attention when something stops. The pump, the filter and the conveyor run in the background, specified once and left alone. That habit is changing. Find out what’s driving the change, and what the next generation of conveying equipment needs to deliver.
Powder conveying: what’s changing and how to adapt
Insights
27/10/2026

The business case for upgrading to Piab's sintered filter

"We ran hundreds of tests, but we couldn't simulate a breakage." That's the line from our film, but robustness is only part of the story. For operations and procurement, the real questions are what a filter does for control, compliance and stable production, and how much effort it takes to switch. Here's how the sintered filter answers each one.
The business case for Piab's sintered filter: traceability, compliance and control
Insights
27/10/2026

From guesswork to control: why spare-part traceability matters in powder handling

In many plants, spare-part knowledge lives in people's heads, on worn labels and in old order confirmations. That works until someone leaves, a label fades or an auditor asks a question no one can answer. For an operations leader, that's a control problem, not a maintenance detail.
From guesswork to control: why spare-part traceability matters in powder handling
Insights
02/10/2026

PFAS in your production line: what the EU restriction means for process equipment

Most conversations about PFAS focus on consumer products like non-stick pans and outdoor jackets. But PFAS are also built into industrial equipment: seals, gaskets, coatings and filter media. For anyone responsible for a production site, the question is no longer whether PFAS will be regulated, but how fast your equipment and supply chain can adapt.
PFAS in your production line: what the EU restriction means for process equipment
Insights
05/08/2026

What is "food-grade" powder handling – and what does it require?

What is "food-grade" powder handling – and what does it require?
View all

Do you need help choosing the right product?

Get free advice from our engineers

Country
I want to receive the latest news on
Conveying solutions

Share article