When a pump upgrade makes sense (and when it doesn't)

Your vacuum pump works fine. It's not broken, and switching to piEVO won't transform your line's performance overnight. The honest starting point: the difference between an older pump and piEVO isn't large. What's different is how it feels to work with it, day-to-day.
piEVO isn't a leap in capability — it's a smoother experience: fewer parts to wrestle with, quicker access when something needs attention, materials that hold up better. If you or your team touch the pump regularly, you'll notice it. If you don't, you may not — and that's a fair conclusion to reach.
What an older setup typically looks like
A conventional vacuum pump is a standalone machine built for fixed mounting and standard servicing. In practice:
- Bolted connections that take longer to open and close, often needing two people
- Several small parts around the exhaust/silencer to track, order, and replace individually
- A layout that isn't always intuitive — reaching in takes a moment of thought
None of this is a flaw exactly — it's just an older approach, and it shows up as small friction each time someone works on the pump.
piEVO: 7 reasons for a smoother experience
Most of these changes came from listening to customers about what was fiddly or time-consuming, then working through those pain points one at a time.
- Quick-swap bayonet interface. One operator can mount or remove the pump in minutes, without tools or a second person.
- Bayonet access on the suction side, too. The suction port cover uses the same click-on, click-off logic — no wrench needed there either.
- Fewer, better parts around the exhaust. Several small plastic components have been consolidated into a single part, in an improved material. Less to track, less likely to feel worn or flimsy.
- Cleaner layout. More compact and easier to read at a glance — less time spent figuring out where to reach in.
- Accessible internals. The exhaust side detaches with four bolts. A cleaning job that used to take two people about an hour can be done by one person in around 20 minutes.
- Compact, powerful ejector. The new 2-stage ejector is twice as powerful as the Si32-3 model, yet 50% smaller — and interchangeable with Si32-3, so a switch can happen gradually.
- Built with room to grow. Quick connectors, gauges, and modular sensor interfaces are part of the design, even though nothing about today's version requires them. If your line moves toward more data-driven operation later, the pump won't need to be swapped out to get there.
None of these are dramatic upgrades individually. Together, they add up to a pump that's simply more pleasant to work with — without closing the door on where things might go next.
piEVO vs. a standard pump
| Dimension | Existing Pump Setup | piEVO |
|---|---|---|
| Performance | Performs as expected at its duty point | Comparable — this isn't where the difference lies |
| Servicing | Bolted connections, typically needs two people | Bayonet access on pump and suction port — one person, no tools |
| Parts around the exhaust | Several small plastic pieces to track and replace | Consolidated into a single, better-material part |
| Cleaning & changeover | Hard-to-reach internals, more time-consuming | Four-bolt access, noticeably quicker for one person |
| Everyday feel | Functional, gets the job done | Cleaner layout, feels more considered to work with |
The honest read: most of this isn't about doing something new — it's the same thing with less friction.
Who notices the difference
- Whoever services the line sees the clearest win — less time, fewer people needed, less hassle with small parts.
- Operations managers see it indirectly: servicing that's quicker and doesn't always need two people's availability.
- Compliance/safety roles: the exhaust improvement is worth a mention, but it's secondary to the servicing story.
- Finance: the case is modest — some time saved per service, fewer worn parts to re-buy. Not a transformative TCO story but it has a foundation for the applications that will come in future for scaling.
When it's genuinely not worth acting on
- Servicing isn't a pain point for you today.
- A major line refresh is already planned within 12 months — fold this into that conversation instead.
- You're mid-capex or in a budget freeze. The case will be just as valid in 6 months.
It's fine — expected, even — for the answer to be "this isn't a priority right now."
If none of these land, piEVO probably isn't worth prioritizing right now. If one or two do, it's worth a conversation with whoever services the pump — not a full line assessment.
Where this leads next
This is deliberately a modest comparison: piEVO is the same pump, made nicer to work with, built so a move toward more data-driven operation later doesn't require starting over. Whether that's worth something to you depends on how much you value that day-to-day ease today. If you’re still not sure the pump is actually the constraint, “Pump performance vs. system performance: what’s actually slowing you down” takes a step back and looks at the whole conveying system.
The business case article in this series looks at whether — and how — that's worth putting a number on, without overstating what's really a usability story.
Discover more insights
Pump performance vs. system performance: what's actually slowing you down

When a pump upgrade makes sense (and when it doesn't)

How best-in-class factories standardize powder handling - and why it works

Stop paying for the “hidden factory” in powder handling

Choose Powder Handling You Won’t Have to Redesign in Three Years