Feedback

Choose your language

Close

Vacuum ejector piPUMP 23

New piPUMP offers vacuum without the frills

Date 11/21/2017

piPUMP 23 is a no-frills version of the premium vacuum ejector piCOMPACT®23.

Taby, Sweden – Piab is introducing piPUMP 23, a powerful vacuum pump aimed at automated industrial procedures involving, for instance, packaging, sheet metal and wood products. The new pump offers the same premium vacuum ejection performance and energy-efficiency as piCOMPACT®23, the company's popular all-in-one vacuum generator. However, not included are the advanced integrated controls and additional features of piCOMPACT®23, resulting in a considerably less expensive vacuum pump for customers who might not require these specialized functions.

Fully configurable, piPUMP 23 is available with either one or two COAX® SX12/SX42 multistage vacuum ejector cartridges, and can be supplied with or without cleanable and replaceable filters in two optional sizes. The pump can be configured for up to three vacuum connections, making it suitable for a variety of applications and industrial settings.

Retained from the piCOMPACT® platform is Piab's proprietary Amplified Blow-Off (ABO) feature, resulting in a more efficient, powerful and energy-saving blow-off. By closing the flow-path of the ejectors during blow-off, the ABO feature ensures that 100% of the compressed air is channelled through to the cups during blow-off, providing a very strong and efficient release, which in turn enables faster production cycles. The feature is also useful for floating suction cups while positioning them in, for instance, ergonomic lifting aids. Customers might also find this feature practical when cleaning suction cups in dusty environments.

Simplified and straightforward, piPUMP 23 is a powerful vacuum generator that is easy to integrate and install in vacuum handling systems used for, for instance, the palletizing of boxes, and the loading, sorting, and transportation of sheet metal and wood products.

About Piab

Established in 1951, Piab designs innovative vacuum solutions that improve the energy-efficiency, productivity, and working environments of vacuum users around the world. As a reliable partner to many of the world's largest manufacturers, Piab develops and manufactures a complete line of vacuum pumps, vacuum accessories, vacuum conveyors and suction cups for a variety of automated material handling and factory automation processes. Piab utilizes COAX®, a completely new dimension in vacuum technology, in many of its original products and solutions. COAX® cartridges are smaller, more energy efficient and more reliable than conventional ejectors, and can be integrated directly into machinery. This allows for the design of a flexible, modular vacuum system. In 2016, Piab completed two strategically important acquisitions, Kenos and Vaculex. Piab is a worldwide organization with subsidiaries and distributors in almost 70 countries. Its headquarters are in Sweden.