“PE”在污水处理厂中是什么意思?

PE stands for Population Equivalent. It is the standard unit used across European wastewater legislation to describe the load a treatment plant must handle.
One PE represents the average organic biodegradable load produced by one person per day – defined as 60 grams of biochemical oxygen demand (BOD₅) over five days.
Why PE, not just population?
A treatment plant serves more than just households. Industrial discharges, food processing facilities, hospitals, and seasonal tourism all contribute to the load. PE allows all of these to be expressed in the same unit. A small dairy might add the equivalent of 5,000 PE to a plant that serves a town of 20,000 people, giving the plant a total design load of 25,000 PE.
Why the 150,000 PE threshold matters
Directive (EU) 2024/3019 uses PE to define which plants are subject to which obligations. The fourth treatment stage requirement applies to plants serving more than 150,000 PE. Smaller plants face other requirements but are not (yet) required to install a quaternary stage.
In Germany alone, roughly 3,000 plants fall within this scope. Across the EU, the number is significantly higher and will grow as member states translate the directive into national law.
Practical implication
For plant managers, the first question is whether their plant is above, at, or close to the 150,000 PE threshold. Plants close to the threshold should plan for the upgrade even if not formally required today – industrial growth or municipal expansion can push them over.
This explainer is referenced from the articles "EU Directive 2024/3019: what the fourth treatment stage means for your plant" and "Building the business case for a fourth-stage upgrade: 20-year thinking in a 20-month decision".
Discover more insights
粉末输送:正在发生哪些变化以及如何适应

升级至 Piab 烧结过滤器的商业论证

从猜测到控制:为什么备件可追溯性在粉末输送中至关重要

生产线中的 PFAS:欧盟限制措施对流程设备意味着什么

构建第四阶段升级的商业论证:在20个月的决策中进行20年的思考

Do you need help choosing the right product?
Get free advice from our engineers