活性炭与臭氧化——第四阶段规划的快速比较

发布于 2026/9/15
活性炭与臭氧化——第四阶段规划的快速比较

The EU directive does not prescribe a specific technology for the fourth treatment stage. The two dominant options are adsorption on activated carbon (powdered or granular) and oxidation by ozone. Each has trade-offs. 

Activated carbon (PAC or GAC) 

  • How it works: micropollutants adsorb onto the high surface area of the carbon.
  • Strengths: well understood, broad spectrum of micropollutants captured, low energy demand, no harmful by-products. 
  • Weaknesses: ongoing consumable cost; dosing reliability depends on robust powder handling (see the cocoa effect); spent carbon must be disposed of or regenerated.  

Ozonation 

  • How it works: ozone oxidizes micropollutants directly in the water.
  • Strengths: no consumable to dose continuously; compact footprint. 
  • Weaknesses: high electricity demand; can form by-products (such as bromate) requiring a downstream biological filter; more complex process control.  

The hybrid trend 

A growing number of plants combine both: ozonation followed by activated carbon polishing, or activated carbon as the main stage with ozone reserved for specific contaminants. The optimal choice depends on influent profile, energy prices, and operational preferences.

Where IB fits 

IB's strength is in the powder handling side – specifically, robust dosing of activated carbon at full plant scale, drawing on experience from activated carbon dosing in waste incineration plants. The operational reliability of the dosing system is often what separates a fourth-stage plant that performs from one that struggles. 
This explainer is referenced from the articles "EU Directive 2024/3019: what the fourth treatment stage means for your plant", "Activated carbon or ozonation? A framework for choosing your fourth-stage technology", and "Building the business case for a fourth-stage upgrade: 20-year thinking in a 20-month decision". 

Discover more insights

Insights
2026/11/11

粉末输送:正在发生哪些变化以及如何适应

在大多数工厂中,只有在出现停机时,粉末输送才会受到关注。真空发生器、过滤器和输送机在后台运行,一次选定后便不再过问。这种习惯正在改变。了解推动这一变化的因素,以及新一代输送设备需要具备哪些能力。
粉末输送:正在发生哪些变化以及如何适应
Insights
2026/11/11

升级至 Piab 烧结过滤器的商业论证

“我们进行了数百次测试,但无法模拟出破损。”这是我们影片中的一句话,但坚固性只是故事的一部分。对于运营成本和采购而言,真正的问题是过滤器如何实现控制、合规性和稳定生产,以及切换需要付出多少努力。以下是烧结过滤器如何逐一解答这些问题。
Piab 烧结过滤器的商业论证:可追溯性、合规性与控制
Insights
2026/11/11

从猜测到控制:为什么备件可追溯性在粉末输送中至关重要

在许多工厂中,关于备件的知识存在于员工的脑海中、磨损的标签上以及旧订单确认单里。在有人离职、标签褪色或审核员提出无人能回答的问题之前,这种方式都还能运作。对于运营负责人而言,这是一个控制问题,而非维护细节。
从猜测到控制:为什么备件可追溯性在粉末输送中至关重要
Insights
2026/11/11

生产线中的 PFAS:欧盟限制措施对流程设备意味着什么

大多数关于 PFAS 的讨论都集中在不粘锅和户外夹克等消费产品上。但 PFAS 也被用于工业设备中:密封圈、垫片、包衣和过滤介质。对于负责生产现场的人员而言,问题不再是 PFAS 是否会受到监管,而是您的设备和供应链能多快适应。
生产线中的 PFAS:欧盟限制措施对流程设备意味着什么
Insights
2026/9/15

构建第四阶段升级的商业论证:在20个月的决策中进行20年的思考

构建第四阶段升级的商业论证:在20个月的决策中进行20年的思考
View all

Do you need help choosing the right product?

Get free advice from our engineers

国家
我希望收到关于…的最新消息
物料输送解决方案

分享文章