Date 01/09/2020
Piab continues the software development of the piFLOW®p SMART software platform, which focuses on ease of use and improved/added functionality
ECU-10 will be phased out and replaced with a new controller ECU-15. With this phase out of ECU-10, there will be one common family of Electrical Control Units, the ECU-15 family, where ECU-15 will be offered to all conveyors and ECU-15S will be part of the piFLOW®p SMART offering.
The main benefit of having the same ECU-platform is that lot of new functionality is added to the “SMART” offering, which can be implemented to the standard ECU as well.
For easy installation and troubleshooting, a check on various functions and components has been added.
Several new monitoring functions are also introduced: