Feedback

Choose your language

Close

piFLOW®i/f 28L vacuum conveyor

Introducing the piFLOW®i/f 28L vacuum conveyor

日付 2020/04/01

Piab is extending the piFLOW®i/f family range with a new vacuum conveyor that allows for larger batch volume.

The new piFLOW®i/f has a 28L body and the possibility for configurations such as double mounting of the piBASIC 400 and 600 pumps on the cover, meaning that the total pump capacity can be increased to 800 or 1200. For example, this will increase production from the current 4 ton per hour (14L and 600 pump) to 7,5 tons per hour with the addition of 2 x piBASIC 600.

 

Piab AB © 2020 個人情報に関する通知

フォローする

ご連絡下さい