Piab strengthens global support for safer, smarter powder handling

Piab is accelerating its vacuum conveying offering to help manufacturers replace manual, labour‑intensive powder handling with safer, fully automated solutions. Building on more than 75 years of industrial experience and a presence in over 25 countries, Piab’s Vacuum Conveying division supports customers in food, pharmaceutical, chemical and other process industries that are looking to improve productivity, uptime and working conditions on their lines.
Many factories still move powders and granules the way they did decades ago – with operators lifting bags, carrying buckets and filling machines by hand. In the article “Moving Manufacturing Forward”, Niclas Dahl, President of Vacuum Conveying, highlights how enclosed vacuum conveying systems automate this “invisible” movement of material to protect operators and secure stable throughput.
By eliminating open transfers, Piab’s systems help reduce dust exposure, minimise ergonomic strain and mitigate contamination and explosion risks in sensitive applications such as food ingredients, pharmaceutical APIs, or even combustible powders.
At the heart of this approach are three clear strengths: Flexible. Reliable. Sustainable. Piab offers a broad, configurable range of vacuum conveyors and material storage solutions that can be tailored to different powders, throughput levels and plant layouts, from premium systems to value‑optimised setups.
Solutions scale from single units to complex multi‑line systems, supported by global application knowledge in segments such as food, pharma, additive manufacturing, and defence.
Reliability and uptime are equally critical. Piab delivers fully integrated systems that automate the entire material handling process, helping customers achieve higher output with consistent quality while minimising unplanned stops. Equipment is designed for fast cleaning and easy service, with accessible components that reduce maintenance time and total cost of ownership.
As manufacturers move towards more planned, data‑driven maintenance, Piab is investing in monitoring and predictive tools that help optimise service intervals and maximize uptime.
Sustainability and a safer work environment run through the entire offering. Enclosed vacuum conveying removes much of the manual handling of heavy or hazardous materials, reducing operator exposure to dust, fumes, and ergonomic strain. Systems are engineered to meet strict standards such as FDA, EHEDG, GMP and ATEX, supporting customers in highly regulated environments.
Optimised pump technology and intelligent controls further help lower energy consumption compared to traditional mechanical conveying methods.
As safety and sustainability requirements continue to rise in automation, Piab’s Vacuum Conveying division remains focused on helping manufacturers work smarter, safer, and more efficiently – making the “invisible” movement of powders a true competitive advantage.
Read the full magazine here: