From dust to downtime: The real costs of poor powder handling

In bulk powder production, your conveying method matters more than you might think. Even small weaknesses and inefficiencies in your material handling can affect output, product quality, compliance and, most importantly, staff health and safety. This article explores common risks across industries, and how they quietly drive up production costs.

In many production environments, material handling is treated as a secondary function. The main investment goes into mixers, tablet presses, filling machines, packaging lines or other high-value equipment. Conveying is typically seen as the practical step that simply moves material from A to B – preferably as efficiently as possible for maximum productivity.

But the way powders, granules or small parts move through your process impacts several areas HSEQ teams care about most. A few examples:

  • How much dust escapes into the production area
  • How often operators need to handle material manually
  • How easy the system is to clean between batches
  • How well the product is protected from contamination

4 common health & safety risks in powder handling

How can poorly suited powder handling methods put operators at risk, in the short and long term? The answer depends on your materials, processes and production environment. But across industries such as food and beverage, pharmaceuticals, chemicals and other powder-based manufacturing, the same types of challenges tend to appear. Here are four common risk factors to look out for in your production plant:

1. Harmful dust exposure

When powders are poured, transferred or conveyed through open systems, dust easily spreads into the surrounding work environment. In some applications, this leads to respiratory irritation or sensitization. In others, the material may be hazardous, potent or otherwise require strict exposure control. Even when dust is not immediately visible, repeated low-level exposure can still contribute to long-term respiratory health problems.

dust exposure in industrial facility
operator empties bucket into coffee roaster - bad ergonomics

2. Poor ergonomics due to manual handling

Does your production environment still rely on operators carrying bags, lifting containers, climbing ladders or manually filling hoppers? This puts long-term physical strain on operators, especially when the work is repetitive, heavy or performed at height. It also places operators closer to exposed material, increasing the risk of dust inhalation or direct contact.

3. Combustible or reactive dust risks

Depending on their chemical and physical properties, some powders introduce additional safety concerns. Fine particles are capable of igniting or contributing to an explosion when airborne in the right concentration and exposed to an ignition source. At-risk materials include certain food ingredients, organic powders, chemicals and metal powders. Because this risk is highly application-specific, dust control becomes especially important in processes where powder can escape, accumulate on surfaces or spread through the work environment.

combustible risk in industrial facilities
spills in industrial facilities - risk of slips

4. Slips and additional exposure caused by spills

Spilled powder doesn’t only reduce output or create waste. It also increases slip risks, as well as other health and safety issues. When material needs to be swept, vacuumed, wiped up or removed from hard-to-reach areas, every unplanned cleanup becomes another potential exposure point. 

The common thread across these risk factors is clear: the more open, manual and intervention-heavy your conveying process is, the more opportunities there are for operators to come into contact with material. For HSEQ teams, reducing these touchpoints is key to keeping exposure under control and maintaining a safe, compliant work environment.

How safety risks increase production costs

The same factors that increase operator exposure typically affect quality and output as well. Dust, spills and repeated manual intervention are tell-tale signs that your material handling is not as controlled or efficient as it could be. And over time, the costs add up:

  • Spills create waste and additional cleaning.
  • Dust emissions increase cleaning needs and risk triggering inspections or stoppages.
  • Manual filling ties up operators and increases the risk of delays or mistakes.
  • Blockages and overflows interrupt production and require hands-on troubleshooting.
  • Residues between batches can lead to cross-contamination or discarded product.
  • Complex cleaning routines take time away from production and depend heavily on operator consistency.

To sum it up, powder handling isn’t just a matter of moving material from one point to another. When the process creates unnecessary exposure, cleanups or interventions, it affects your entire production environment – from operator wellbeing and hygiene control to output, waste and batch quality. 

FILL OUT THE FORM BELOW TO DOWNLOAD THE GUIDE (In English)

Want to uncover hidden material handling bottlenecks – and find smarter ways forward?

Dust, spills and cleaning challenges are often symptoms of a wider material handling issue. In our guide, “Is your material handling holding back your production?”, we walk you through common signs that your current setup is limiting safety, hygiene, uptime and production flow. You’ll also get practical guidance on what to consider when assessing cleaner, more efficient ways to move material through your plant.

FILL OUT THE FORM TO DOWNLOAD THE GUIDE

Country
I want to receive the latest news on