Achieving a leadership position in the Fresh Dairy Products market would not be possible without the hygienic, efficient transporting of key ingredients. This is why Danone Poland was interested in finding a cost-effective conveying solution that could quickly and reliably transfer powders like moisture-absorbing whey and non-free-flowing starch.
The company chose to install two of vacuum partner Piab’s piFLOW®p conveyors to integrate into its automatic powdering station.
Reliability and efficiency concerns have been met with fluidization now integrated into the powdering station with the new conveyors, allowing starch and whey to flow more freely from the vacuum receiver. Another benefit of the piFLOW p Series was its space-saving attribute, as Danone Poland was dealing with limited free space in its facility.