Metal Additive Manufacturing
Metal additive manufacturing is a quickly emerging industry with strong technology focus to continue improving its productivity and efficiency while maintaining high quality and adhering to health and safety standards. Raw materials used are primarily metal powders like titanium, nickel, stainless steel, cobalt, iron, tungsten carbide, all with their individual challenges.

What is additive manufacturing?
Metal additive manufacturing, also known as metal 3D printing, is an advanced manufacturing technique that involves building three-dimensional objects layer by layer using metal powders. This process is quite different from traditional subtractive manufacturing methods, where the material is removed from a solid block to create the final product. In metal additive manufacturing, the object is created by adding the material layer by layer until the desired shape is achieved.
How does 3D printing with metal work?
The metal 3D printer selectively fuses or sinters the metal powder layer by layer, following the sliced design. Various techniques are used for metal additive manufacturing, such as selective laser melting (SLM), electron beam melting (EBM), or binder jetting where a high-energy source is used to selectively melt or fuse the metal powder.
Our applications for metal additive manufacturing
Operators usually feed the printers, the sieves, or hoppers manually from small bottles. Therefore, the process relies heavily on manual labor and exposes the employee to hazardous metal powder dust and heavy lifting. Automating the process enables higher productivity, as well as safety and an ergonomic working environment for the employees.
These solutions result in a higher level of productivity, avoid product scrap, and establish an ergonomic working environment.
In metal additive manufacturing, Piab vacuum conveyors can be used to enable automation of the whole process, but particularly used in the following process steps:

Filling the 3D printer with metal powder
Piab vacuum conveyors pick up the virgin or recovered metal powder directly from a sieve/metal drum or hopper and feed the 3D printer. The removal can also be done directly from the overflow container.
Filling a sieve or hopper with metal powder
Piab vacuum conveyors can feed the sieve or hopper directly from the original manufacturer's drum or vat when pre-sieving is required or recover metal powder from the 3D printer's overflow vessel. Our conveyors for metal additive manufacturing can be integrated into portable sieving solutions due to their ease of assembly and light weight, allowing the same conveying and sieving solution already used for printers.
Recovering metal powder from the printer
Metal powders are both expensive and hazardous, so proper powder recovery from the printer is critical. Piab's piFLOW® vacuum conveyors can transport metal powder from the printer to the original manufacturer's sieve or drum/container via a closed system to increase productivity and ensure the workers’ safety. It is possible to recover metal powder from the overflow hopper and build the plate directly from the printer or by using a Piab feed pipe.
piFLOW® by Piab: Our conveying solutions for metal additive manufacturing
With our extensive experience in material handling, Piab's vacuum conveyors have long been an efficient solution for handling powders. Here is what our Piab premium conveyors offer:
- a stainless steel (ASTM 316L) housing
- Piab's highly efficient COAX® vacuum technology
- ATEX dust and gas certification
- built-in automatic filter cleaning
- powder handling up to ca. 8 kg/liter [500 lbs./ft3] bulk density and an impressive throughput
- minimal footprint
Piab provides the greatest flexibility by working with various additive manufacturing technologies, such as Powder Bed Fusion and Binder Jetting.
Our piFLOW® conveyors can be easily integrated to existing machine parks and production lines. We offer seamless integration of automated vacuum conveying solutions into any powder-based manufacturing process. The piFLOW® conveyors:
- avoid exposure to hazardous materials of technicians while not compromising on production efficiency
- enhance overall efficiency and productivity through automated powder handling
- reduce supply chain disruptions by offering a more streamlined manufacturing process
- ensure that the material doesn't degrade, and powder mixes don't segregate during the manufacturing process
- minimize the risk of contamination through a closed-loop system, with easily cleanable and sanitizable conveying equipment.
With Piab’s products, you can connect the dots within the Additive Manufacturing production line with ease!
Metal additive manufacturing and the automation of powder handling
Shortened development cycle
Metal additive manufacturing is a method used both for prototyping and increasingly for serial production of metal parts. It gives the possibility to design and produce previously impossible components or use custom alloys. Component delivery gets faster due to a shortened development cycle. Metal Additive manufacturing reduces supply chain disruptions and contributes to reduced part weight.
Powder handling automation
Given the high growth rates and increasing opportunities in the additive manufacturing industry, powder handling automation is key to establishing the technology as a standard production process. However, many process steps are still manual. This includes the loading of the production equipment with the appropriate metal powder. Furthermore, the use of vacuum conveying technologies can help protect people, products, and the environment.
Ideal vacuum conveyors
Piab's premium conveyors have long been efficiently supporting AM proceses. They are equipped with a stainless steel (ASTM 316L) housing and feature the COAX® vacuum technology and built-in filter cleaning. Configurations are available to meet ATEX Dust and Gas requirements. Based on Piab's in-house tests on various metals and alloys, Piab conveyors can handle powders with a bulk density of 8 kg/liter [500 lbs/ft3] with an impressive throughput.
Adaptable solutions
Working with a variety of Additive Manufacturing technologies, such as Powder Bed Fusion and Binder Jetting, Piab offers the greatest flexibility in integrating automated vacuum conveying solutions into any powder-based manufacturing process. This adaptability ensures seamless integration and improved efficiency, allowing manufacturers to optimize their production lines and remain competitive in the industry.
Piab and the metal additive manufacturing industry: Strong success stories
Enhancing Innovation: Piab & IB Joint Expertise
IB is a renowned leader in the manufacturing of highly customized machines and an accomplished supplier for powderhandling solutions. This collaboration enhances Piab's in-house expertise, product portfolio, and offerings in the additive manufacturing industry, focusing on advanced metal powder conveying solutions designed to meet the evolving needs of our clients.
Piab & IB’s solutions support KSB's growth
KSB, a premier provider of pumps, valves, and systems across diverse applications reduced their powder handling setup time, using the IB ultrasonic sieving station MPS30 with an integrated Piab piFLOW® vacuum conveyor. They increased productivity and efficiency and reduced the need for manual labor.
Previously we did manual powder handling and then sieving the powder and transferring it back to the [3D printing] machine, which was very timeconsuming: [...] took up half of a day. Right now we can just remove the powder from the machine, sieve it, and refill the machine in less than 30 minutes.
Solukon relies on vacuum conveyors from Piab in its new Powder Collection Unit
Solukon and Piab have established an exciting collaboration, where innovative vacuum conveyor technology is boosting the efficiency and safety of powder-based 3D printing. The Solukon Powder Collection Unit (SFM-PCU for short) is a fully automated powder collection solution for metal powders. With the help of the piFLOW®i vacuum conveyor from Piab, Solukon makes powder handling simpler and safer right after depowdering.
IB Sieving Stations
Ultrasonic screening for printers with large building chambers
The MPS 30 from IB Additive is an ultrasonic screening station with integrated pneumatic conveying for printers with large build chambers.
It is highly reliable, enabling used powder to be fed directly from the building chamber of the 3D printer via the integrated Piab vacuum conveying system.
In 2023, Piab Group acquired IB Verfahrens- und Anlagentechnik GmbH & Co. KG, a company specializing in customer-specific systems for bulk material handling.


Ultrasonic screening for small build chambers
IB Additive’s MPS5 is an ultrasonic screening station with integrated pneumatic conveying for printers with small build chambers. It is a pinter-independent, process-stable, powerful and compact solution for powder recovery.
Sieving station for metal powder handling via containers
The MPS X1 from IB Additive is an effective solution for powder recovery from IB Additive. It enables the feeding of already used powder and the return transport of the recycled powder via existing containers.
Download the MPS X1 manual here


Piab & Höganäs: In partnership with a metal powder producer
Piab has set a partnership with Höganäs, a Swedish company producing a variety of metal powders.
Through this partnership, we offer big bag/flexbag unloading stations with integrated vacuum conveying for more sustainable ways to work with metal powders. We contribute to industrialization, reduce manual handling, and optimize the amount of powder used in industrial processes.
Get help choosing your ideal conveying equipment!
Find out what applies to your raw materials and products! Fill in the form to get free, personal advice from our engineers as well as comparisons with other technologies to find the best solution for your needs.