Warners plc, a magazine and brochure printer based in the UK, purchased a new, state-of-the-art binder. The binder was selected for its high productivity level, and so an out-of-the-box solution to minimize heat generation and noise was needed.
Six P6010 pumps from Piab were installed for vacuum and blow functions on the new binder. By equipping two pumps with the Vacustat control system, an integrated air saving function, the system minimizes energy consumption by switching pumps on and off depending on how many are needed.
In addition to reducing heat and noise, the new system from Piab has saved the company costs associated with installation and maintenance time.