A company handling car glass (side windows) was looking for a vacuum solution with energy saving system that would function efficiently even when there was water on the glass.
The company installed two PMAT Vacustat units and measured the difference in compressed air consumption using two digital flow meters.
The compressed air consumption was reduced with almost 94% (!), from 95 Nl/min to 5.83 Nl/min. The actual energy cost was thereby reduced by €44.94 per week, and the investment in Piab products had paid for itself in just over 6 weeks