A world leader in the pharmaceutical industry had only a small space in which to transfer granular ingredients from fluid bed dryers to sterile containers. The company required an automated solution that was easy to operate and compact enough to fit within tight parameters.
The company purchased Piab’s vacuum conveyor, which is fitted to a trolley that moves fluidly between cells.
This vacuum conveor is smaller in size than the equipment previously used, opening up more room on the manufacturing floor. It is very easy to clean and requires no tools for stripping or re-assembly. The company is pleased with the increased ease of use and plans to purchase more conveyors in the near future.