Feedback

Choose your language

Close

Does the unit come with any type of control?

The unit has a pneumatic control which controls the suction and discharge time as well for fluidization.

It can also be without control, in that case the end user will need to provide the sequence of operation – PLC control.

Electric/pneumatic valve unit can be provided ( to convert the electrical signal to a pneumatic output to signal the Piab)

Piab AB © 2019 Privacy notice

Follow us

Contact us