Date 6/18/2012
piFLOW®f is designed for customers that do not want to compromise between price, technical performance and energy consumption.
piFLOW®f is optimized for the food industry. All parts that are in contact with the conveyed material are FDA compliant. Nevertheless, it is still a cost efficient alternative, both from the capacity point of view, but, also in comparison with mechanical conveying methods. The full opening gives an instant discharge, i.e. increased material throughput.
Apart from its design with the full opening, vacuum is produced in the most energy efficient way, namely through utilizing COAX® cartridges. The COAX® cartridges are smaller, more efficient and more reliable than conventional ejectors, which allows for the design of a flexible, modular and efficient vacuum system. A vacuum system based on COAX® technology can provide your customer with three times more vacuum flow than conventional systems, while reducing energy consumption.
”The new piFLOW®f design makes it possible to double the conveying capacity for many materials, compared to traditional conveyors. That it is also a food grade product makes it interesting in a big global market”, says Josef Ramslöv, Vice President Material Handling Division.
Like all other conveying machines that Piab offers the market – piFLOW® is ATEX Dust classified.
Established in 1951, Piab designs innovative vacuum solutions that improve the energy-efficiency, productivity, and working environments of vacuum users around the world. As a reliable partner to many of the world's largest manufacturers, Piab develops and manufactures a complete line of vacuum pumps, vacuum accessories, vacuum conveyors and suction cups for a variety of automated material handling and factory automation processes. Piab utilizes COAX®, the next dimension in vacuum technology, in many of its original products and solutions. COAX® cartridges are smaller, more energy efficient and more reliable than conventional ejectors, and can be integrated directly into machinery. This allows for the design of a flexible, modular vacuum system. Piab has a worldwide organization with subsidiaries and distributors in more than 50 countries, with headquarters in Sweden.
Ed McGovern, Vice President Sales & Business Development, North America
Tel: +1 (781) 337 7309
E-mail: ed.mcgovern@piab.com