Feedback

Choose your language

Close

Super flexible piGRIP®FXI suction cup

New piGRIP® suction cup offers super flexibility

Date 11/7/2018

Internal “locking” retainer perfects the grip of the long super soft lip on Piab’s piGRIP®FXI suction cup.

Taby, Sweden – Piab is extending its offering of piGRIP® suction cups, adding a new cup that enables maximum flexibility. The piGRIP®FXI is the latest member of the company's popular configurable piGRIP® suction cup range.

With a longer, thinner and super soft lip, the new suction cup is designed to provide an excellent grip even on highly perforated or heavily patterned surfaces that might prove challenging for other cups. Its extra sealing capability makes the cup suitable for safe handling of surface leaking materials with, for instance, wrinkled and textured surfaces, and for porous materials such as corrugated paper.

Available in four different sizes offering diameters between 30mm and 84mm, the piGRIP®FXI suction cup is suitable for a broad range of automated vacuum handling applications.

"The FXI cup is able to handle everything from the highly decorative designer packaging used in the cosmetics industry, the pharmaceutical industry's blister packages and lids/covers with printed relief text to the highly textured components used in the building trade," says Josef Karbassi, Vice President of Piab's Automation Division.

The integrated high flow retainer prevents the super soft and extra long lip from curling or folding when applied on surfaces. The retainer ensures that the flexible lip is not being sucked into the cup instead of spreading over the surface of handled objects.

The piGRIP®FXI suction cup is available in two alternative softness versions, scoring 30 and 18 respectively, on the Shore A durometer hardness scale. The softest 18 shore version is considerably softer than previously available parts and ensures maximum flexibility.

Made in recyclable and FDA and EU approved materials recommended for food handling, the piGRIP®series offers 40 different fittings together with a generic interface.

About Piab

Piab provides smart solutions for the automated world, helping thousands of end users and machine producers in e-commerce logistics, food, pharma, automotive and other manufacturing industries to improve energy-efficiency, productivity and working environments. With 430 employees and SEK 1 bn in sales 2017, Piab is a global organization, serving customers in almost 70 countries from a network of subsidiaries and distributors. By leveraging the ongoing technological development in automation and robotics, and targeting high-growth segments and geographies, Piab's vision is to become the global leader in gripping and moving solutions.