If you are having trouble logging in, please clear your cookies 

Feedback

Choose your language

Close

PR piGRIP BGI

Improved design on bag lip for piGRIP® suction cup

Date 6/2/2014

Better gripping performance ensures higher productivity.

Piab introduces the next generation of piGRIP® bag lips, known as "BGI". These lips include an internal retainer piece as well as three additional diameter sizes. The bag lips are ideal for handling different types of bag materials, especially hard-to-handle thin bag material, such as plastic film. The six diameter sizes now at 25, 34, 41, 48, 63 & 80 mm provides a larger range of sizes for choosing the exact cup for the handling application.

Our first generation piGRIP® bag lips "BG" were developed to handle most types of bags and pouches much better than any other available suction cup on the market. The special lip design in combination with the rigid and strong piGRIP® bellows/body allows for bag handling speeds and accelerations never used before in automation equipment for bags/pouches. Beside regular plastic bags for dry food (e.g. chips), the new piGRIP® bag lips were designed to have an excellent grip on stand-up-pouches filled with liquid or dry/wet food/substances.

The range of diameter sizes now allows for very small and/or oblong narrow flexible packages (fast-food ketchup packs) to be handled by the smallest 25 mm size. The largest size, 80 mm, addresses the need for handling heavy bags or sacks such as animal feed sacks.

The new retainer piece prevents thin bags or films from being drawn into the cup, thus improving the grip performance as well as eliminating marks on the thin bag materials. The lip material and the retainer piece are made of FDA approved materials.

A new much stronger bonding solution between the lip and bellows will prevent lips from coming off during working cycles, even for extremely rough conditions (high speed and greasy environments). The new locking sleeve, in terms of a retainer, guarantees the lip will stay in position. Cost savings are possible from exchangeable lips, thanks to the new locking solution – you only need to replace the lip and not entire bag cup-fitting.

About Piab

Established in 1951, Piab designs innovative vacuum solutions that improve the energy-efficiency, productivity, and working environments of vacuum users around the world. As a reliable partner to many of the world's largest manufacturers, Piab develops and manufactures a complete line of vacuum pumps, vacuum accessories, vacuum conveyors and suction cups for a variety of automated material handling and factory automation processes. Piab utilizes COAX®, a completely new dimension in vacuum technology, in many of its original products and solutions. COAX® cartridges are smaller, more energy efficient and more reliable than conventional ejectors, and can be integrated directly into machinery. This allows for the design of a flexible, modular vacuum system. Piab is a worldwide organization with subsidiaries and distributors in almost 70 countries. Its headquarters are in Sweden.