Skip to content
BX suction cups made of double-strength Duraflex® in combination with Piab's COAX® vacuum generation technology have enabled Tradicional Panadera to palletise different carton formats with a single gripper.
Using Piab's Kenos® KVG grippers, Officina Meccanica Sestese SpA designed and manufactured an end-of-line packaging machine installed at a leading company in Southeast Europe, a manufacturer of components for the furniture industry.
Using Piab's B52XP suction cups and piCOMPACT23 SMART pump, Cob-Solution designed and built a system to handle the picking and opening of cardboard boxes at Rao Farmaceutici, Sicilian veterinary pharmacy that is investing in e-commerce and selling throughout all Europe.
With a maximum payload of one kilogram for the Wyzo sidebot, the weight of the gripper is critical. Therefor Piab's featherweight Mini Cobot gripper (MCG) at 270 gr, fits perfectly.
A unique, intelligent, solution that automates the intralogistics and material handling from inbound to the finished, delivered kitted items at the individual production lines has been created...
Using Piab's suction cups and vacuum pumps, Tecno Pack SpA has designed and built grippers...
dm is currently the largest drugstore in Europe. At their distribution center a large part of the pallets is depalletized with...
Forvet SpA has created end-of-arm tools that allow handling glass sheets of different sizes...
The machine builder GO GmbH were looking for an “all-in-one” gripper solution that can be used to stack both loose and packaged furniture parts on and off pallets, as well as the pallets themselves. The solution was...
With 32,500 cycles per day, 24 hours a day, seven days a week, this application is one of those with the highest number of...
To automaticaly remove extruded aluminium profiles from cassettes in high-bay warehouses, JAM Automation created...
Thanks to Piab's Kenos® KVG area vacuum gripper, an extreme variability of sizes and surfaces can be managed, using just a single gripper. This allowed...
Different product types can’t be compared. Do you want to remove the existing products?