Feedback

Choose your language

Close

How can I set the vacuum level when handling different objects which individually need different levels?

The multistage COAX® ejector is designed so the maximum vacuum level can be adjusted by the compressed air feed pressure. By using a piSAVE optimize, you can set the specific vacuum level needed and the piSAVE optimize will adjust the feed pressure to the pump accordingly. You will never use more compressed air than needed in the application. Please also try the piSAVE optimize calculator to see the actual energy saving by doing this.

Piab AB © 2019 Legalnotice

Follow us

Contact us