Lifting solutions for parcel carrier terminals

Parcel carrier terminals

Situation

At parcel carrier terminals there is always manual handling of parcels at some point. Manual handling is often the only alternative when loading and unloading containers or trailers, sorting parcels between pallets, cages and conveyors.

In this type of operation manual handling is typically high tempo in work postures that often cause injuries, if not performed with some lifting aid.

Keeping in mind the weight of parcels can often be around 40 kg, manual handling affects your body. Repetitive strain injuries and severe injury to, for example, spine and shoulders is common. The result is what you don’t want - high sick absence, low productivity and dissatisfied workers.

Solution

Vaculex® has developed and implemented lifting technology to solve the manual handling problems at parcel carrier terminals. The results are ergonomic vacuum lifting solutions that potentially increase productivity while still minimizing the risk for repetitive strain injuries and other injuries to, for example, the spine.

Integrating Vaculex® ergonomic lifting equipment into the existing handling system is easy. In cases where there is limited space such as low head room, narrow passages and confined areas, Vaculex® has a flexible solution.

A common challenge at the receiving dock is unloading loose loaded containers and trailers. This is one of the most physically demanding jobs at parcel carrier terminal, due to heavy lifting, bad posture, high intensity and a work environment that is also often in need of other improvements.

Vaculex® ergonomic vacuum lifting equipment for parcel carrier terminals offer solutions for:

Caixa
Caixa

As encartuchadeiras (montador de caixas) são projetadas para construir caixas e recipientes a partir de peças brutas planas feitas de papelão flexível ou material similar. O vácuo é usado...

Caixa e bandeja
Caixa e bandeja

Os montadores de caixa montam caixas a partir de folhas planas de material corrugado. As caixas montadas são então preenchidas com os produtos ou com caixas individuais e preparadas para o processo…

Manuseio de pacotes flexíveis
Manuseio de pacotes flexíveis

Material de embalagem flexível é o termo genérico para pacotes macios feitos de película, material laminado ou papel. As formas populares são bolsas verticais, sacolas, sachês e envelopes. Esses...…

Rotulagem
Rotulagem

Dois métodos bastante comuns de aplicar rótulos com vácuo são a rotulagem por pressão e a rotulagem pneumática. As máquinas de rotulagem por pressão aplicam rótulos pontuais sensíveis à pressão. Um…

Posicionamento
Posicionamento

O uso de robôs para posicionar produtos em caixas e transferir as caixas e os produtos entre diferentes estações nas linhas de embalagem é muito comum em todas as indústrias. Robôs de pick-and…

Palletizing boxes and parcels
Palletizing and depalletizing

Piab has developed Vaculex® specialized lifting solutions for palletizing which reduce repetitive strain injuries as well as improving productivity.

Elevador ergonômico
Elevador ergonômico

A redução de lesões e o aumento da produtividade são muitas vezes alcançados com a ajuda de dispositivos de elevação ergonômicos. Esse tipo de equipamento permite que um ou dois operadores levantem…

Piab AB © 2018 Informação legal

Siga-nos

Contate-nos