Date 26/03/2013
Piab, a leading supplier of industrial vacuum technology, offers its patented COAX® technology in a new simplified integration platform called piCHIP. COAX® is the most energy efficient ejector technology based on a multi-stage concept for creating vacuum with compressed air.
The lightweight piCHIP unit is flexible enough to surface mount quickly on a variety of materials. Having both the compressed air and vacuum ports on the same side makes it a natural for integration. If performance needs to be increased due to changes in your process, the piCHIP can be modified to double the unit's output quite easily for faster response.
With its almost silent operation, the piCHIP is ideal for clean room operations. Medical and electronic industries are best suited to use this product in their vacuum applications.
Because COAX® cartridges are up to twice as fast as other cartridges and provide three times more flow than a conventional ejector with the same air consumption, the piCHIP is able to provide a high performance even at low or fluctuating feed pressures (1-6 bar). Additionally, piCHIP vacuum units begin producing vacuum immediately when the pressure valve is turned on, making maximum use of the compressed air and consuming significantly less energy than traditional vacuum pumps.
Established in 1951, Piab designs innovative vacuum solutions that improve the energy-efficiency, productivity, and working environments of vacuum users around the world. As a reliable partner to many of the world's largest manufacturers, Piab develops and manufactures a complete line of vacuum pumps, vacuum accessories, vacuum conveyors and suction cups for a variety of automated material handling and factory automation processes. Piab utilizes COAX®, a completely new dimension in vacuum technology, in many of its original products and solutions. COAX® cartridges are smaller, more energy efficient and more reliable than conventional ejectors, and can be integrated directly into machinery. This allows for the design of a flexible, modular vacuum system. Piab is a worldwide organization with subsidiaries and distributors in more than 50 countries. Its headquarters are in Sweden.
Häla El Sheemy Washbrook, Vice President Marketing and Communications Manager
Tel: +46 (0) 8 630 25 74
E-mail: hala.e.washbrook@piab.com