New DURAFLEX® friction cups

New friction cup range keeps every sheet safe

Date 02/05/2016

Six new cups keep a tight hold on extra thin and shaped sheet metal at higher stroke rates.

Taby, Sweden – Expanding its family of DURAFLEX® friction cups, Piab is making sure that they meet emerging market requirements, and are able to offer the best and safest possible solution for any type of sheet metal handling. Safer handling of often oily sheets offers the opportunity to increase the number of strokes per minute in stamping, cutting, bending, and punching machines, making for more cost-effective and productive press shops.

The new range comprises three BFFT (Bellows Flat Friction Thin) cups, a design specifically developed to provide ultimate grip on extremely thin sheets without the risk of denting the delicate surface. Sheets of thicknesses down to 0.6-0.8mm can be safely handled by the new friction cups.

Complementing the BFFT cups are three DCF (Deep Concave Friction) cups, designed to meet the requirements of the next production step within, for instance, the automotive industry, when the flat metal sheets are turned into curved body parts. The three new DCF cups provide maximum hold on parts with a concave or convex surface.

”These new cups are broadening the performance range of our friction cup family, which already offers so many important advantages compared with other solutions. For instance, our friction cups are extremely durable and will keep their excellent grip performance throughout their entire life, whereas competing cups often deteriorate quickly,” says Josef Karbassi, Vice President of Piab's Automation Division.

Combining the properties of polyurethane with those of rubber, Piab's friction cups display exceptional elastic memory and press oil resistance, enabling them to keep their shape and remain in good working order. Competing cups are prone to losing their memory i.e. their shape with increasing age and usage.

In addition, Piab offers a multitude of accessories including many different fittings meeting various standards, advanced plastic fittings of reduced weight, mounting brackets and quick release T-adapters.

About Piab

Established in 1951, Piab designs innovative vacuum solutions that improve the energy-efficiency, productivity, and working environments of vacuum users around the world. As a reliable partner to many of the world's largest manufacturers, Piab develops and manufactures a complete line of vacuum pumps, vacuum accessories, vacuum conveyors and suction cups for a variety of automated material handling and factory automation processes. Piab utilizes COAX®, a completely new dimension in vacuum technology, in many of its original products and solutions. COAX® cartridges are smaller, more energy efficient and more reliable than conventional ejectors, and can be integrated directly into machinery. This allows for the design of a flexible, modular vacuum system. Piab is a worldwide organization with subsidiaries and distributors in almost 70 countries. Its headquarters are in Sweden.

More information

Häla El Sheemy Washbrook, Vice President Marketing and Communications Manager
Tel: +46 (0) 8 630 25 74
E-mail: hala.e.washbrook@piab.com

Piab AB © 2018 Legal notice

Follow us

Contact us