Feedback

Choose your language

Close

piPUMP

Efficiency and easy installation in a neat format – piPUMP

Date 16/06/2014

Vacuum pump designed for small parts pick and place

Piab, a leading supplier of industrial vacuum technology, offers its patented COAX® technology in a new small sized ejector called piPUMP MICRO.  COAX® is the most energy efficient ejector technology based on a multi-stage concept for creating vacuum with compressed air.

piPUMP MICRO is truly easy-to-buy and easy-to-mount and use. A handy configurator tool on Piab’s website, www.piab.com, allows the user to select the vacuum characteristics along with a few options for filtration and connections. 

The piPUMP can be used for small centralized systems but perhaps even more suitable for semi-decentralized systems, i.e., a few units creating vacuum supporting a few small cups each. Thanks to very low weight and small dimension it can also be used as a fully decentralized ejector on a Delta robot for example.

The small footprint of the unit provides flexibility in mounting and use. Installation is a breeze with push-in connections and a common feed for compressed air, regardless of the number of units chosen. The central exhaust allows the exhaust to be drawn away in clean room environments. 

Because COAX® cartridges are up to twice as fast as other cartridges and provide three times more flow than a conventional ejector with the same air consumption; the piPUMP MICRO is able to provide a high performance even at low or fluctuating feed pressures (0,1-0,6 MPa).  Additionally, piPUMP MICRO vacuum units begin producing vacuum immediately when the pressure valve is turned on, making maximum use of the compressed air and consuming significantly less energy than traditional vacuum pumps.

About Piab

Established in 1951, Piab designs innovative vacuum solutions that improve the energy-efficiency, productivity, and working environments of vacuum users around the world. As a reliable partner to many of the world's largest manufacturers, Piab develops and manufactures a complete line of vacuum pumps, vacuum accessories, vacuum conveyors and suction cups for a variety of automated material handling and factory automation processes. Piab utilizes COAX®, a completely new dimension in vacuum technology, in many of its original products and solutions. COAX® cartridges are smaller, more energy efficient and more reliable than conventional ejectors, and can be integrated directly into machinery. This allows for the design of a flexible, modular vacuum system. Piab is a worldwide organization with subsidiaries and distributors in more than 50 countries. Its headquarters are in Sweden. 

More information

Häla El Sheemy Washbrook, Vice President Marketing and Communications Manager
Tel: +46 (0) 8 630 25 74
E-mail: hala.e.washbrook@piab.com

 

Piab AB © 2019 Privacy notice

Follow us

Contact us