Feedback

Choose your language

Close

COAX® cartridge Di16-2

Dust-proof innovation for Piab’s COAX® technology

Date 23/03/2015

Piab introduces a new COAX® vacuum ejector that is ideal for applications where there is dust or dirt present. This MINI size cartridge is ideal for Piab's VGS™3010 vacuum gripper system, a decentralized vacuum system that features a suction cup and an efficient multi-stage air driven vacuum pump integrated in a single unit, called a "Gripper."

In dusty/dirty environments, such as in packaging where corrugated dust is prevalent, this new COAX® Di16-2 dust-proof cartridge performs very well. Usually, in these places, vacuum filters cannot be used due to their propensity to fill up with dust and reduce the overall effectiveness of the vacuum system. The new COAX® Di16-2 is a two-stage cartridge without flap valves. Dust and dirt has a free path through the ejector nozzles, eliminating the risk for clogging- even in extreme applications, such as high humidity in combination with dust. The COAX® Di16-2 provides vacuum levels down to 70-kPa at a feed pressure of 6 bar.

COAX® is an ejector technology based on a multi-stage concept for creating vacuum with compressed air. By integrating the internal components of a multi-stage vacuum pump into a vacuum cartridge, COAX® allows for a smaller, more efficient, more reliable and highly flexible technology. This flexibility is particularly helpful for users who plan to design a modular system to address specific application needs.

 

The majority of Piab's current vacuum pumps feature COAX® technology and are compact, simple to install and generate minimal noise.

About Piab

Established in 1951, Piab designs innovative vacuum solutions that improve the energy-efficiency, productivity, and working environments of vacuum users around the world. As a reliable partner to many of the world’s largest manufacturers, Piab develops and manufactures a complete line of vacuum pumps, vacuum accessories, vacuum conveyors and suction cups for a variety of automated material handling and factory automation processes. Piab utilizes COAX®, a completely new dimension in vacuum technology, in many of its original products and solutions. COAX® cartridges are smaller, more energy efficient and more reliable than conventional ejectors, and can be integrated directly into machinery. This allows for the design of a flexible, modular vacuum system. Piab is a worldwide organization with subsidiaries and distributors in almost 70 countries. Its headquarters are in Sweden. 

More information

Häla El Sheemy Washbrook, Vice President Marketing and Communications Manager
Tel: +46 (0) 8 630 25 74
E-mail: hala.e.washbrook@piab.com 

Piab AB © 2019 Legalnotice

Follow us

Contact us