Choose your language

Close

ウェブサイトを快適にお使いいただくため、Piab のウェブサイトはcookieを使用しています。
設定を変更されない場合、cookieを受け取ることに同意されたとみなします。
Read more


piCOMPACT™ MICRO

世界最速のオールインワン式エジェクター

日付 2014/03/19

ピアブ社は、piCOMPACT™ の種類を増やしました。COAX®技術をベースにした機能的なエジェクターシステムです。

By working at low feed pressure and maximizing the utilization rate of the compressed air, the COAX® ejectors reduce energy consumption for manufacturers while increasing productivity and reliability. Products in the piCOMPACT™ range are ideal for pick-and-place operations where efficient handling of small, heavy parts is crucial, common for electronics, semiconductor, plastics, metal, small packaging, pick and place and robotic integration.

Using Piab’s unique COAX® cartridges, the world's smallest multistage vacuum ejector, the piCOMPACT™ range provides three times more vacuum flow than similar products. This reduces energy consumption by 30-50 percent compared with traditional ejectors, resulting in substantial sustainability benefits as well as energy and cost savings. By offering an increased vacuum flow, piCOMPACT™ ejectors strengthen product grip to increase pickup speed, minimize product damage and reduce waste. piCOMPACT™ also allows faster release of products from the suction cups onto the production line for efficiency gains.

The intelligent Energy-Saving (ES) function effectively turns off the compressed air usage when set vacuum level is achieved. An additional feature connected to the ES function, ACM, eliminates the issue of "motor-boating", where the vacuum generator cycles on and off repeatedly in case of leakage. ACM automatically senses if ES is needed or not. It can also be used for monitoring when it is time to replace worn out suction cups. With integrated direct operating bullet valves for on/off and blow-off as part of the complete piCOMPACT™ package, reliability, uptime and speed of operation can be ensured. piCOMPACT™'s user-friendly signal and energy saving setting means there are no risks for any mistakes in setting parameters for efficient vacuum operation. 

Products in the updated piCOMPACT™ range are smaller and lighter than conventional ejectors, reducing the total weight of vacuum handling systems. This innovative design allows vacuum systems to move more quickly to increase production capacity.

 “Vacuum ejectors today are essential components for an uncounted number of general manufacturing and automation applications across a wide range of industries, with hundreds of specific product requirements. Across the board, manufacturers are seeking improved performance together with reduced total cost of ownership while always considering their impact on the environment,” said Häla El Sheemy Washbrook, Vice President Marketing and Communication, Piab. “Energy consumption is a key consideration for manufacturers when looking to reduce costs of a complete vacuum system. Working at low pressures with efficient COAX® technology, the piCOMPACT™ range increases productivity for small product handling applications, saving money and reducing a manufacturers’ carbon footprint.”

The piCOMPACT™ vacuum ejectors are available in a broad selection to fit with a variety of systems, including those that require very low feed pressure or extra deep vacuum levels. In addition, the compact ejectors can be easily integrated into existing production lines with no modifications required, and can be quickly configured to meet individual manufacturing needs.

ピアブについて

1951年に創立されたピアブは、革新的な真空技術を持って、エネルギーの効率化、生産性の向上など、お客様の作業環境を改善に寄与し続けております。世界中のお客様の信頼できるパートナーとしてピアブは、自動マテリアルハンドリング、工場自動化工程等の用途向けに、バキュームポンプ、バキュームアクセサリー、バキュームコンベア、サクションカップを開発し、ご提供しております。ピアブは真空技術としては全く新しい発想によって、COAX®カートリッジを開発し、多くのアプリケーション、ソリューション向けにご提供しております。COAX®カートリッジは、従来型のエジェクターと比較すると、小型かつエネルギー効率に優れ、また信頼性が高いエジェクターであります。これにより、柔軟でモジュール式の真空システムの設計が可能になりました。ピアブは、スウェーデンに本社を置き、世界50ヶ国以上に子会社と代理店を持つ国際的なネットワークを持った会社です。

ご質問のある場合は、下記までご連絡下さい。

info-jp@piab.com

 

 

Piab AB © 2017 法律上の表示

フォローする

ご連絡下さい