Feedback

Choose your language

Close

Piab's Vaculex® vacuum lifter for barrels and kegs

Lift barrels ergonomically with Vaculex® lifters

Date 2/21/2018

Piab's ergonomic Vaculex® vacuum lifter helps boost brewery productivity and saves backs.

Taby, Sweden – A booming business, microbreweries are also characterized by heavy manual work for an often very limited number of staff. It takes two to lift and turn a barrel and a forklift truck to stack barrels ready for delivery. The result – high risk of strain injuries and expensive machine investments.

A vacuum-operated barrel handling solution can change that. Promising to make breweries of all sizes more productive and more ergonomically friendly workplaces, the Vaculex® VL will lift, rotate and stack heavy and bulky kegs or barrels in one motion. It enables parts of the process to be handled by one member of staff and without the need of a forklift.

Suitable for handling half barrels (50-60 liters), an ergonomic Vaculex® VL has been specifically developed for the brewery industry. Powered by an electric vacuum pump the Vaculex® VL will lift any barrel allowing workers to manouever and transfer these with ease and without fear of strain or repetitive injuries. Enabling procedures to be carried out in space-restricted areas, Piab offers unique and flexible solutions where ceiling height, narrow and confined areas with limited available working space may be an issue. Low profile crane systems, monorails and carbon fibre arms are examples of how Piab provides users with innovative answers to challenging environments.

Offering an ergonomic and safe working environment, Vaculex® VL enables breweries to operate more efficiently. For instance, as barrels are often filled from the underside, they need to be turned upside down as well as lifted during the process, and then lifted for stacking. Weighing up to 165 lbs a piece, this is a back-breaking job even for two workers, but an easy task for an ergonomic Vaculex® lifter operated by one brewery employee.

A complete range of spare parts and helpful accessories - such as a handy remote control, a noise reducing hood and an energy-saving system for automatic pump turn-off during inactivity - coupled with outstanding after-sales support and maintenance enable customers to rest assured that they will be working with ease before, during and after purchasing a Vaculex® lifting solution.

 

About Piab

Established in 1951, Piab designs innovative vacuum solutions that improve the energy-efficiency, productivity, and working environments of vacuum users around the world. As a reliable partner to many of the world's largest manufacturers, Piab develops and manufactures a complete line of vacuum pumps, vacuum accessories, vacuum conveyors and suction cups for a variety of automated material handling and factory automation processes. Piab utilizes COAX®, a completely new dimension in vacuum technology, in many of its original products and solutions. COAX® cartridges are smaller, more energy efficient and more reliable than conventional ejectors, and can be integrated directly into machinery. This allows for the design of a flexible, modular vacuum system. In 2016, Piab completed two strategically important acquisitions, Kenos and Vaculex®. Piab is a worldwide organization with subsidiaries and distributors in almost 70 countries. Its headquarters are in Sweden.

More information

Häla El Sheemy Washbrook, Vice President Marketing and Communications Manager
Tel: +46 (0) 8 630 25 74
E-mail: hala.e.washbrook@piab.com

Piab AB © 2019 Privacy notice

Follow us

Contact us