Other accessories

If the application, for example, requires that the exhaust air is led into the ventilation system to avoid any particles from the conveyed products leaking out in the surrounding environment, a central exhaust can be fitted to the pump. If here is a need to decrease the noise level, there is an option with a free-flow silencer. The silencer fits the central exhaust, connected with a straight pipe fitting D=75. vacuum filter can be mounted on the feed adapter so that the carrying air into the conveyor is clean and not contaminated with particles from the surrounding environment.