Vacuum conveyors for powder & bulk

Vacuum conveyors for powder & bulk

Vacuum is used with great advantage in order to convey dry powder products through dedicated pipe systems. Piab's vacuum conveying systems are built of strong components of high quality. Our objective is to offer solutions that help our customers raise their productivity.

Production of food, pharmaceuticals and chemical products demands the highest possible degree of safety as to hygiene and operation. Piab's C series of vacuum conveyors has been developed as an answer to the severe requirements of operational safety and hygiene in the food, pharmaceutical and chemical industries.

Vacuum conveyor training tutorial

 

This tutorial will overview some of the more basic parts of the Piab conveying system. The explanation begins at the top of the conveyor (pump) and concludes at the base (bottom valve).

View tutorial   (Adobe Flash player is needed.)

Piab quality standards

Piab offers conveyors for ATEX applications. These conveyors are type examined according to ATEX by a third party. Piab has a quality management system which fulfils the high standards that is required for delivering ATEX equipment on a regular basis.

Since there are special safety requirements for equipment and health protection for workers in potentially explosive atmospheres, the EU has created legislation called the ATEX directives. Equipment that is certified according to the ATEX directive 94/9/EC has to be designed in a way that it cannot cause an explosion during its intended use.

The conveyors fulfil the requirements for the following ATEX zone classification for dust: zone 21 and 22 on the outside and zone 20 on the inside.

Piab’s conveyors that are classified for use in potentially explosive atmospheres have specific features.

  • All seals/rubber parts between the machine’s sheet metal parts are made of dissipative (antistatic) materials.
  • All larger plastic parts are made of dissipative (antistatic) materials.
  • As a consequence of this, only antistatic variants of filters and fluidization cones  are used.

An ATEX-certified conveyor is delivered with CE Declaration of conformity and CE marking that clearly states the ATEX classification and contains the EX symbol.
EX II 1/2 D c +80°C 0ºC <= Ta <= 60ºC

The U.S. Food and Drug Administration (FDA) issues a Code of Federal Regulations that regulates what materials can be used in contact with foodstuffs and pharmaceuticals.  Piab’s C and UC series of vacuum conveyors consist solely of materials that are in accordance with FDA requirements.
One of the objectives of the United States Department of Agriculture (USDA) is to ensure the quality of food products and the safety of the consumer. USDA reviews and accepts process equipment for dairy products. Piab follows the guidelines from USDA.

 

 

Pharmaceutical – C conveyors

The pharmaceutical industry has a very high demand for cleanliness as well as for health and safety. Since many of the different powders produced in the pharmaceutical industry are hazardous or considered being a safety risk, Piab designed its range of conveyors to meet these special demands. Piab conveyors work with an enclosed vacuum ...

Consumer & food – C conveyors

The most common application within consumer and food industries is conveying ingredients from big or small bags to different process steps in production or conveying the final product to the packaging line. Piab’s range of conveyors can handle powders with particle sizes down to 0.5 micron, capacities up to 10 tons/hour and distances up ...

Chemical – C conveyors

The chemical industry often handles aggressive and hazardous powders that require specially designed equipment. Piab conveyors work with an enclosed vacuum system which ensures the highest level of working environment for the operator. Piab conveyors are ATEX Dust compliant. Piab quality standards Typical applications Painting/paint ...

General – piFLOW™i

The General industry often handles abrasive powders that require specially designed equipment. Our conveyors are designed with Stainless Steel body (ASTM 304) to resist wear of parts. Piab conveyors are ATEX Dust compliant. Piab quality standards Typical applications Powder and granules transfer Form-fill-seal Big Bag loading and ...

ATEX conveyors

Since there are special safety requirements for equipment and health protection for workers in potentially explosive atmospheres the EU has created legislation for this called the ATEX directives. (ATEX is an abbreviation for Atmosphère Explosible). Equipment that is certified according to the ATEX directive 94/9/EC has to be designed in ...

Other accessories

If the application, for example, requires that the exhaust air is led into the ventilation system to avoid any particles from the conveyed products leaking out in the surrounding environment, a central exhaust can be fitted to the pump. If here is a need to decrease the noise level, there is an option with a free-flow silencer. The ...

Spare parts

The vacuum conveyor is reliable and requires a minimum of maintenance. It is, however, necessary to regularly change some of the parts to maintain maximum productivity.