Chemical & plastics
The chemicals and plastics industries are spending a lot of money on maintaining and purchasing vacuum pumps and vacuum-related equipment. In the chemical industry the pumps are exposed to a lot of aggressive chemicals that require resistant vacuum pump materials. Vacuum automation solutions in the plastics industry have to face challenges like unloading of high temperature parts with textured surfaces but also mark-free and PWIS-free (Paint Wetting Impariment Substances) requirements.
Piab has over 30 years of experience of powder and granules transfer through vacuum conveying. We handle particle sizes from 0.5 micron. The conveying capacity reaches up to 10 tons/hour and the conveying distance up to 30 meters. However, capacity and distance is very dependent on the properties of the conveyed material. In some cases ...
The use of robots for placing products in cartons and transfer of cartons and products between different stations in the packaging lines is very common in all industries. High speed pick-and-place robots for placing small items like candy and cookies in packages are often combined with a visual observation system for identifying products ...
Palletizing is the process of placing packages on a pallet alternatively removing them from a pallet (depalletizing). Palletizing machines use vacuum pumps, suction cups and other pneumatic components. These machines typically pick up multiple boxes at a time and place them on a stack (or remove them from a stack). Today, because of the ...
During vacuum forming (thermo-forming), the ambient atmospheric pressure is used to form/press pre-heated plastic sheets over a mold. Air is rapidly evacuated from the mold by a vacuum pump and a vacuum tank will give extra initial power/flow. A deep end-vacuum is also needed to get the right "definition" on the finished ...
Piab has over 30 years of experience of powder and granules transfer through vacuum conveying. We handle particle sizes from 0.5 micron. The conveying capacity reaches up to 10 tons/hour and the conveying distance up to 30 meters. However, capacity and distance is very dependent on the properties of the conveyed material. In some cases ...
Blank Destacker has been developed specifically for feeding sheet blanks into fully automatic lines. Blanks of metal (magnetic or non-magnetic), plastic, wood or cardboard are separated from a stack and fed into the line. Vacuum pumps and cups are used to “pick-up/separate” and feed. It is important to choose the right type of suction ...
Reducing injury and increasing productivity are often accomplished with the aid of ergonomic lifting devices. This type of equipment allows one or two operators to lift, move and manipulate large and small objects with vacuum. Unlike a robot, the lifting device requires an operator to position the part being handled. Reliable safety ...
The application is typically to transfer material from a Big Bag into a suction pipeline. We use a Feed Adaptor with a universal interface to connect to the Big Bag unloading system. The feed adaptor is designed to optimize the flow of the material in the pipeline with multiple valves for adjusting the airflow. This feature is essential ...
Handling hazardous powders require a completely closed system to avoid exposure. Piab´s conveying system operates with negative pressure, ensuring no contamination of the surrounding environment even if there is a minor leakage. The system can be wet down before maintenance or cleaning operations. Piab has over 30 years of experience of ...
In several industries there are clamping fixtures where suction cups are used to hold parts during assembly, forming, cutting or other machining operations. In many cases the cycle times are long and an energy-saving system is therefore recommended.
Advantages with Piab
Reduced energy consumption with COAX® technology and ...
Conveying powder and granules can in some cases generate an explosive dust/air mixture. To eliminate the risk of dust explosion, Piab meets the international ATEX standard. This is done by removing all sources of ignition from the system, i.e. electric and electrostatic. Piab has over 30 years of experience of powder and granules ...
After plastic parts have been formed in injection molding machines, they are typically removed from the mold with the help of suction cups and vacuum pumps that are usually attached to a robot arm. The temperature of the molded plastic parts can be quite high.
Advantages with Piab
Reduced energy consumption with COAX® technology and ...
The use of specialized machines for high speed pick-and-place of small items with suction cups is very common in the electronics and consumer industries. This application is typically characterized by short cycle times, high acceleration forces and large variations on the parts to be handled.
Advantages with Piab
Reduced energy ...
Vacuum conveying is an excellent alternative to manual operations such as carrying or lifting or mechanical operations such as belt conveyors, when it comes to working environment. Piab’s systems eliminate manual operation steps and at the same time reduce the amount of maintenance and dust contamination with positive results for the ...
The very first part of the packaging process might require a filler tube or a hopper to be loaded with the product. Vacuum conveyors are used for this purpose. They convey the material to be packaged into a hopper or filler tube where it is then delivered into pouches and sealed. When the machine is of horizontal form-fill-seal design, ...
Piab systems are designed to meet requirements specified by international standards such as 3-A Sanitary Standard and FDA (Food and Drug Administration). Piab vacuum conveyors are developed in accordance with USDA guidelines and meet the demands of dairy, food and other farm producers. Piab has over 30 years of experience of powder ...
For special projects where customized design is required, Piab uses a global network of engineers. Piab has 30 years of experience in customized designs with several hundred projects worldwide. We have designed and tested solutions for all industries using powders, granules or small products. Our focus when designing vacuum conveying ...
To automatically rack stamped metal panels or other large parts. The panels are loaded into shipping racks for movement to next process in the line. The size and weight of the panels make it difficult for operators to manually handle and racking them. Robots are used and typically equipped with a vision system. A retracting level ...
Piab has over 30 years of experience of powder and granules transfer through vacuum conveying. We handle particle sizes from 0.5 micron. The conveying capacity reaches up to 10 tons/hour and the conveying distance up to 30 meters. However, capacity and distance is very dependent on the properties of the conveyed material. In some cases ...
During the manufacturing of laminated products like veneer sheets and plastic hull of a a boat, vacuum is used to eliminate bubbles and thereby increase the material strength.
Advantages with Piab
No service required on Piab vacuum pumps
Energy-saving function can easily be incorporated
Easy adjustable vacuum level
Easy to ...
Removal of liquid from a solid material with the aid of vacuum. Drying with vacuum is often used when products are sensitive to heat (cause oxidation), to recover toxic material or if the final product has to be extremely dry.
Advantages with Piab
No service required on Piab vacuum pumps
Easy adjustable vacuum level
Easy to ...
In final assembly of certain machines/products like cars and refrigerators, fluid systems are filled before the machine/product leaves the manufacturing facility. To speed up the process of filling fluids the air is evacuated from the volume that is to be filled. A second vacuum is required that is applied at the end of the filling ...
Vacuum is used in test equipment for printed circuit boards to press the board against the electrical test points. The vacuum creates an even pressure/force over the entire board. Vacuum and suction cups are also used to clamp/hold parts in several industries during quality control by measuring the critical dimensions of ...
Tire and rubber manufacturers use vacuum for material handling and forming applications. The process of molding tires includes a vacuum assist that helps rubber form inside a mold cavity. Tires and rubber slabs are also handled by means of vacuum pumps and suction cups.
Advantages with Piab
Reduced energy consumption with COAX® ...
To achieve an effective degassing of oils and other liquids, vacuum is used. The largest possible surface area is exposed to vacuum.
Advantages with Piab
No service required on Piab vacuum pumps
Easy adjustable vacuum level
Easy to install
Automotive manufacturing facilities designate an enclosed booth area for painting vehicles and vehicle parts. Vacuum conveyors are used to convey the powdered paint primer into large mixing tanks. From the tanks the powder is conveyed to the paint spray guns where it is then applied to the vehicle. Conveyors are also used to collect any ...
Vacuum is used to achieve a wider differential pressure of a filter material to get a more effective and faster filtration. Typically used in applications where liquids are separated from solids.
Advantages with Piab
No service required on Piab vacuum pumps
Easy adjustable vacuum level
Easy to install
Vacuum is applied on mold cavities to give molded products a better definition.
Advantages with Piab
No service required on Piab vacuum pumps
Low noise level
Easy to install
Vacuum is used to reduce the point of boiling so that an optimised temperature and pressure can be applied during evaporation or crystallization of liquids.
Advantages with Piab
No service required on Piab vacuum pumps
Easy adjustable vacuum level
Easy to install